Hello community,
Our customer ask us about reason of the specification change about VDD_SNVS_IN/VDD_HIGH_IN maximum
voltage range from 3.3V to 3.6V from imx6quad to imx6quadplus.
In EB810. it can show in section 18 Power.
By this document, it seems that reason is a max power consumption on VDD_SOC and NVDD_DRAM.
If both typical and maximum voltage are changed, I can understand.
But typical voltage keep a 3.0V.
Why does it change only maximum voltage range to 3.6V by max power consumption of VDD_SOC and
NVDD_DRAM?
Best regards,
Ishii.
解決済! 解決策の投稿を見る。
Hi Ishii
it changed for more power design flexibility as allows more freedom
for input voltage and possible input voltage changes (instability) during power up
sequence. There is no special need to increase typical voltage as it increase power consumption.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Ishii
it changed for more power design flexibility as allows more freedom
for input voltage and possible input voltage changes (instability) during power up
sequence. There is no special need to increase typical voltage as it increase power consumption.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Igor
Thank you for your quick reply.
I understood why it was changed.
Best regards,
Ishii.