IMX6QP LPDDR2 Calibration Issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6QP LPDDR2 Calibration Issue

950 Views
nxf53093
NXP Employee
NXP Employee

Hi All,

We need some help for iMX6QP LPDDR2 Dual-channel bringing up. Here are details below.

Board ID: SCH-29181 REV B

DDR Device: Micron - EDBA164B2PR 

Programming aids: MX6QP_SabreSD_LPDDR2_register_programming_aid_v1_3

DDR stress tester: V3.0

We have generated initial file 6QP.inc from aids, which only changed tMRD and some pad resistance, and we use 2 channel, 2 cs per channel.  MR1 Value(HEX)=C201

Now, channel 0 can calibrate successfully at 400MHz, but channel 1 fail calibration from 300 to 400. Any can give some help?

============================================
DDR Stress Test (3.0.0)
Build: Dec 14 2018, 14:12:06
NXP Semiconductors.
============================================

============================================
Chip ID
CHIP ID = i.MX6 Dual/Quad (0x63)
Internal Revision = TO2.0
============================================

============================================
Boot Configuration
SRC_SBMR1(0x020d8004) = 0x00100000
SRC_SBMR2(0x020d801c) = 0x12000000
============================================

ARM Clock set to 1GHz

============================================
DDR configuration
BOOT_CFG3[5-4]: 0x01, Fixed 2x32 map.
DDR type is LPDDR2 in 2-channel fixed 2x32 mode. Showing channel0 info only
Data width: 32, bank num: 8
Row size: 14, col size: 10
Both chip select CSD0 and CSD1 are used
Density per chip select: 512MB
Density per channel: 1024MB

NOTE:In order to run calibration in LPDDR2 2-channel fixed 2x32 mode both (all)
channels must be selected to test, if not, calibration will fail requiring you
to re-start the test. You can also choose to skip calibration.
============================================

Current Temperature: 27
============================================

DDR Freq: 396 MHz

LPDDR2 2 CHANNELS
Note: Array result[] holds the DRAM test result of each byte.
0: test pass. 1: test fail
4 bits respresent the result of 1 byte.
result 0001:byte 0 fail.
result 0011:byte 0, 1 fail.

Starting Read calibration...

Test channel 0
ABS_OFFSET=0x00000000 result[00]=0x1111
ABS_OFFSET=0x04040404 result[01]=0x1111
ABS_OFFSET=0x08080808 result[02]=0x1111
ABS_OFFSET=0x0C0C0C0C result[03]=0x1111
ABS_OFFSET=0x10101010 result[04]=0x1111
ABS_OFFSET=0x14141414 result[05]=0x1111
ABS_OFFSET=0x18181818 result[06]=0x1000
ABS_OFFSET=0x1C1C1C1C result[07]=0x0000
ABS_OFFSET=0x20202020 result[08]=0x0010
ABS_OFFSET=0x24242424 result[09]=0x0000
ABS_OFFSET=0x28282828 result[0A]=0x0010
ABS_OFFSET=0x2C2C2C2C result[0B]=0x0000
ABS_OFFSET=0x30303030 result[0C]=0x0000
ABS_OFFSET=0x34343434 result[0D]=0x0000
ABS_OFFSET=0x38383838 result[0E]=0x0000
ABS_OFFSET=0x3C3C3C3C result[0F]=0x0000
ABS_OFFSET=0x40404040 result[10]=0x0000
ABS_OFFSET=0x44444444 result[11]=0x0010
ABS_OFFSET=0x48484848 result[12]=0x0000
ABS_OFFSET=0x4C4C4C4C result[13]=0x0000
ABS_OFFSET=0x50505050 result[14]=0x0000
ABS_OFFSET=0x54545454 result[15]=0x0000
ABS_OFFSET=0x58585858 result[16]=0x0000
ABS_OFFSET=0x5C5C5C5C result[17]=0x0000
ABS_OFFSET=0x60606060 result[18]=0x0000
ABS_OFFSET=0x64646464 result[19]=0x0000
ABS_OFFSET=0x68686868 result[1A]=0x0010
ABS_OFFSET=0x6C6C6C6C result[1B]=0x0111
ABS_OFFSET=0x70707070 result[1C]=0x0111
ABS_OFFSET=0x74747474 result[1D]=0x1111
ABS_OFFSET=0x78787878 result[1E]=0x1111
ABS_OFFSET=0x7C7C7C7C result[1F]=0x1111

Byte 0: (0x18 - 0x68), middle value:0x40
Byte 1: (0x48 - 0x64), middle value:0x56
Byte 2: (0x18 - 0x68), middle value:0x40
Byte 3: (0x1c - 0x70), middle value:0x46
Test channel 1
ABS_OFFSET=0x00000000 result[00]=0x1111
ABS_OFFSET=0x04040404 result[01]=0x1111
ABS_OFFSET=0x08080808 result[02]=0x1111
ABS_OFFSET=0x0C0C0C0C result[03]=0x1111
ABS_OFFSET=0x10101010 result[04]=0x1111
ABS_OFFSET=0x14141414 result[05]=0x1111
ABS_OFFSET=0x18181818 result[06]=0x1111
ABS_OFFSET=0x1C1C1C1C result[07]=0x1111
ABS_OFFSET=0x20202020 result[08]=0x1111
ABS_OFFSET=0x24242424 result[09]=0x1111
ABS_OFFSET=0x28282828 result[0A]=0x1111
ABS_OFFSET=0x2C2C2C2C result[0B]=0x1111
ABS_OFFSET=0x30303030 result[0C]=0x1111
ABS_OFFSET=0x34343434 result[0D]=0x1111
ABS_OFFSET=0x38383838 result[0E]=0x1111
ABS_OFFSET=0x3C3C3C3C result[0F]=0x1111
ABS_OFFSET=0x40404040 result[10]=0x1111
ABS_OFFSET=0x44444444 result[11]=0x1111
ABS_OFFSET=0x48484848 result[12]=0x1111
ABS_OFFSET=0x4C4C4C4C result[13]=0x1111
ABS_OFFSET=0x50505050 result[14]=0x1111
ABS_OFFSET=0x54545454 result[15]=0x1111
ABS_OFFSET=0x58585858 result[16]=0x1111
ABS_OFFSET=0x5C5C5C5C result[17]=0x1111
ABS_OFFSET=0x60606060 result[18]=0x1111
ABS_OFFSET=0x64646464 result[19]=0x1111
ABS_OFFSET=0x68686868 result[1A]=0x1111
ABS_OFFSET=0x6C6C6C6C result[1B]=0x1111
ABS_OFFSET=0x70707070 result[1C]=0x1111
ABS_OFFSET=0x74747474 result[1D]=0x1111
ABS_OFFSET=0x78787878 result[1E]=0x1111
ABS_OFFSET=0x7C7C7C7C result[1F]=0x1111

ERROR FOUND, we can't get suitable value !!!!
dram test fails for all values.

Error: failed during ddr calibration

Labels (1)
0 Kudos
Reply
1 Reply

843 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

  Are there differences in PCB layout for the LPDDR2 channels?

  Also, customers can use the following aid tool:

https://community.nxp.com/docs/DOC-95089 

Have a great day,

Yuri

 

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 Kudos
Reply