IMX6Q opencl 和opengl 使用的GPU是分别是哪个?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6Q opencl 和opengl 使用的GPU是分别是哪个?

949件の閲覧回数
stevenhuang
Contributor III

在IMX6Q平台上,有一个2D 的gpu和3D 的gpu, opencl 和opengl 使用的都是3D的gpu嘛? g2d 是不是可以选择使用某一个gpu?

ラベル(2)
0 件の賞賛
1 返信

382件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi

Triple Play graphics inside the i.MX6 consists of three Vivante GPU cores – GC2000 for graphics and OpenCL, GC320 for composition and GC355 for OpenVG. Each core works seamlessly together to ensure QoS and efficient work-load balance for best-in class reliability and performance. The differentiated cores allow the composition engine to offload all 2D/composition functions from the GPU to save power and allow the GPU to focus on rendering amazing 3D HMIs and configurable instrument clusters.

You can select the API for 2D if you want to use it.

Regards

0 件の賞賛