IMX6Q mipi LCD ghost image

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX6Q mipi LCD ghost image

1,149 次查看
ivychend
Contributor I

      1、Basic information

cpuIMX6Q  android:4.4.2   kernel:linux3.0.5     mipi interface ips LCD

2、problem description

After machine start, when I stay at an UI for more than three minutes. There will be an obvious ghost image(ghost shadow, in chinese:残影).Like stay at setting for 3 minutes

4F0B476D2624B34442B1707D7A735FB9.jpg

Then we can see the setting ghost image at the screen

B6548D9B2F32E055D640778C7414437D.jpg

How to solve this probem? Thanks

标签 (4)
0 项奖励
回复
3 回复数

959 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Jeff

this could be related to this specific lcd usage (for example some

power up sequence is needed), so one can try to get support from

lcd vendor.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

959 次查看
ivychend
Contributor I

Hi igor

I have checked power up sequence and data written to LCD IC for many times. The IC vendor of LCD used the same data to write to screen and it worked fine. Difference is IC vendor use other platform. Furthermore, the LCD works fine in MTK platform. So, there may be some problems in imx6q DSI source code

0 项奖励
回复

959 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Jeff

one can try to check lcd timings and adjust them in driver described

in Chapter 6 MIPI DSI Driver attached Linux Manual.

~igor

0 项奖励
回复