I'm using KK4.4.3_2.0.0-ga release. This release is based on the L3.10.53 kernel. When I use MFGTool2 to download *.img into eMMC of my custom board, the download process stops after printing debug messge "VGEN3: disabling". One of the debug message shows "mmcblk3: unknown partition table", it seems eMMC can't be partitioned. Please kindly advise. Also, based on L3.10.53 kernel version, how to build ram uboot and kernel for MFGTool2? Thanks.
U-Boot 2014.04 (Jan 05 2015 - 14:54:36)
CPU: Freescale i.MX6Q rev1.5 at 792 MHz
CPU: Temperature 31 C, calibration data: 0x57f4ea69
Reset cause: POR
Board: MX6-SabreSD
I2C: ready
DRAM: 1 GiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
No panel detected: default to Hannstar-XGA
Display: Hannstar-XGA (1024x768)
In: serial
Out: serial
Err: serial
Found PFUZE100 deviceid=10,revid=21
Net: Phy not found
PHY reset timed out
FEC [PRIME]
Boot from USB for mfgtools
Use default environment for mfgtools
Run ootcmd_mfg: run mfgtool_args;bootz ${loadaddr} ${initrd_addr} ${fdt_addr};
Hit any key to stop autoboot: 0
Kernel image @ 0x12000000 [ 0x000000 - 0x5093d0 ]
## Loading init Ramdisk from Legacy Image at 12c00000 ...
Image Name: fsl-image-mfgtool-initramfs-imx6
Image Type: ARM Linux RAMDisk Image (gzip compressed)
Data Size: 7377681 Bytes = 7 MiB
Load Address: 00000000
Entry Point: 00000000
Verifying Checksum ... OK
## Flattened Device Tree blob at 18000000
Booting using the fdt blob a 0x18000000
Using Device Tree in place at 18000000, end 1800f1a6
Starting kernel ...
Booting Linux on physical CPU 0x0
Linux version 3.10.53+g496fbe0 (fsl64@fsl64) (gcc version 4.8.1 (GCC) ) #2 SMP Sat Jul 4 19:16:53 CST 2015
CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d
CPU: PIPT / VHPT nonaliasing data cache, VIPT aliasing instruction cache
Machine: Freescale i.MX6 Quad/DualLite (Device Tree), model: Freescale i.MX6 Quad SABRE Smart Device Board
cma: CMA: reserved 320 MiB at 3c000000
Memory policy: ECC diabled, Data cache writealloc
PERCPU: Embedded 8 pages/cpu @81528000 s8768 r8192 d15808 u32768
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 260096
Kernel command line: console=ttymxc0,115200 rdinit=/linuxrc g_mass_storage.stall=0 g_mass_storage.removable=1 g_mass_storage.idVendor=0x066F g_mass_storage.idProduct=0x37FF g_mass_storage.iSerialNumber= enable_wait_mode=off
PID hash table entries: 4096 (order: 2, 16384 bytes)
Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
Inode-cache hash table entries: 5536 (order: 6, 262144 bytes)
Memory: 1024MB = 1024MB total
Memory: 690396k/690396k available, 358180k reserved, 0K highmem
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
vmalloc : 0xc0800000 - 0xff000000 (1000 MB)
lowmem : 0x80000000 - 0xc0000000 (1024 MB)
modules : 0x7f000000 - 0x80000000 ( 16 MB)
.text : 0x8000800 - 0x80c08604 (12290 kB)
.init : 0x80c09000 - 0x80c5b240 ( 329 kB)
.data : 0x80c5c000 - 0x80cad180 ( 325 kB)
.bss : 0x80cad180 - 0x80d0f714 ( 394 kB)
SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
Hierarchical RCU implementation.
NR_IRQS:16 nr_irqs:16 16
L310 cache controller enabled
l2x0: 16 ways, CACHE_ID 0x410000c7, AUX_CTRL 0x32070000, Cache size: 1048576 B
sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655ms
CPU identified as i.MX6Q, silicon rev 1.5
Console: colour dummy device 80x30
Calibrating delay loop... 1581.5 BogoMIPS (lpj=7905280)
pid_max: default: 3768 minimum: 301
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
Setting up static identity map for 0x80639f00 - 0x80639f58
CPU1: Booted secondary processor
CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
CPU2: Booted secondary processor
CPU2: thread -1, cpu 2, socket 0, mpidr 80000002
CPU3: Booted scondary processor
CPU3: thread -1, cpu 3, socket 0, mpidr 80000003
Brought up 4 CPUs
SMP: Total of 4 processors activated (6324.22 BogoMIPS).
CPU: All CPU(s) started in SVC mode.
devtmpfs: initialized
pinctrl core: initialized pinctrl subsystem
regulator-dummy: no parameters
NET: Registered protocol family 16
DMA: preallocated 256 KiB pool for atomic coherent allocations
Use WDOG1 as reset source
syscon 20c8000.anatop: regmap [mem 0x020c8000-0x020c8fff] registered
vdd1p1: 800 <--> 1375 mV at 1125 mV
vdd3p0: 2800 <--> 3150 mV at 3000 mV
vdd2p5: 2000 <--> 2750 mV at 2425 mV
cpu: 725 <--> 1450 mV at 1150 mV
vddpu: 725 <--> 1450 mV
vddsoc: 725 <--> 1450 mV at 1175 mV
syscon 20e0000.iomuxc-gpr: regmap [mem 0x020e0000-0x020e0037] registered
syscon 21bc000.ocotp-ctrl: regmap [mem 0x021bc000-0x021bffff] registered
hw-breakpoint: found 5 (+1 reserved) breakpoint an` 1 watchpoint registers.
hw-breakpoint: maximum watchpoint size is 4 bytes.
imx6q-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver
bio: create slab <bio-0> at 0
mxs-dma 110000.dma-apbh: initialized
usb_otg_vbus: 5000 mV
usb_h1_vbus: 5000 mV
wm8962-supply: no parameters
mipi_dsi_pwr_on: no parameters
sensor-supply: 3300 mV
i2c-core: driver [max17135] using legacy suspend method
i2c-core: driver [max17135] using legacy resume method
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
i2c i2c-0: IMX I2C adapter registered
i2c i2c-1: IMX A2C adapter registered
i2c i2c-2: IMX I2C adapter registered
Linux video capture interface: v2.00
pps_core: LinuxPPS API ver. 1 registered
pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
PTP clock support registered
imx-ipuv3 2400000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
imx-ipuv3 2800000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(0,5), 5F(6,7)
mxc_mipi_csi2 21dc000.mipi_csi: i.MX MIPI CSI2 driver probed
mxc_mipi_csi2 21dc000.mipi_csi: i.MX MIPI CSI2 dphy version is 0x3130302a
MIPI CSI2 driver module loaded
Advanced Linux Sound Architecture Driver Initialized.
cfg80211: Calling CRDA to update world regulatory domain
pureg-dummy: `o parameters
Switching to clocksource mxc_timer1
NET: Registered protocol family 2
TCP established hash table entries: 8192 (order: 4, 65536 bytes)
TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
TCP: Hash tables configured (established 8192 bind 8192)
TCP: reno registered
UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
NET: Regiptered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registerd udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
Trying to unpack rootfs image as initramfs...
Freeing initrd memory: 7200K (82c01000 - 83309000)
hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available
imx6_busfreq busfreq.16: DDR medium rate not supported.
Bus freq driver module loaded
futex hash table entries: 1024 (orde.'¢b²ªª²åÑ?
VFS: Disk quotas dquot_6.5.2
Dquot-cache hash table entries: 1024 (order 0, 4096 bxtes)
NFS: Registering the id_resolver key type
Key type id_resolver registered
Key type id_legacy registered
jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
fuse init (API version 7.22)
msgmni has been set to 2002
io scheduler noop registered
io scheduler dea`line registered
io scheduler cfq registered (default)
imx-weim 21b8000.weim: WEIM driver registered.
mxc_mipi_dsi 21e0000.mipi: i.MX MIPI DSI driver probed
MIPI DSI driver module loaded
mxc_sdc_fb fb.1: registered mxc display driver ldb
imx-ipuv3 2800000.ipu: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)
Console: switching to colour frame buffer device 128x48
mxc_hdmi 20e0000.hdmi_video: Detected HDMI controller 0x13:0xa:0xa0:0xc1
fbcvt: 1920x1080@60: CVT Name - 2.073M9
mxc_sdc_fb fb.32: registered mxc display driver hdmi
mxc_sdc_fb fb.33: registered mxc display driver lcd
mxc_sdc_fb fb.33: ipu0-di0 already in use
mxc_sdc_fb: probe of fb.33 failed with error -16
mxc_sdc_fb fb.34: registered mxc display driver ldb
imx-sdma 20ec000.sdma: no iram assigned, using external mem
imx-sdma 20ec000.sdma: loaded firmware 1.1
imx-sdma 20ec000.sdma: initialized
pfuze10-regulator 1-0008: Full lay: 2, Metal lay: 1
pfuze100-regulator 1-0008: FAB: 0, FIN: 0
p`uze100-regulator 1-0008: pfuze100 found.
SW1AB: 300 <--> 1875 mV at 1375 mV
SW1C: 300 <--> 1875 mV at 1375 mV
SW2: 800 <--> 3300 mV at 3300 mV
SW3A: 400 <--> 1975 mV at 1500 mV
SW3B: 400 <--> 1975 mV at 1500 mV
SW4: 800 <--> 3300 mV at 3150 mV
SWBST: 5000 <--> 5150 mV at 5000 mV
VSNVS: 1000 <--> 3000 mV at 3000 mV
VREFDDR: 750 mV
VGEN1: 800 <--> 1550 mV at 1500 mV
VGEN2: 800 <--> 1550 mV at 1500 mV
VGEN3: 1800 <--> 3300 mV at 2800 mV
VGEN4: 1800 <--> 3300 mV at 1800 mV
VGEN5: 1800 <--> 3300 mV at 3000 mV
VGEN6: 1800 <--> 3300 mV at 3300 mV
Serial: IMX driver
2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 58) is a IMX
console [ttymxc0] enabled
serial: Freescale lpuart driver
imx sema4 driver is registered.
[drm] Initialized drm 1.1.0 20060810
[drm] Initialized vivante 1.0.0 20120216 on minor 0
brd: module loaded
loop:j½Õ±loaded
Wait for CR ACK error!
Wait for CR ACK error!
Wait for CR ACK error!
Wait for CR ACK error!
Wait for CR ACK error!
Wait for CR ACK error!
Wait for CR ACK error!
Wait for CR ACK error!
Wait for CR ACK error!
Wait for CR ACK error!
Wait for CR ACK error!
Wait for CR ACK error!
Wait for CR ACK error!
Wait for CR ACK error!
Wating for RX_PLL lock time out
------------[ cut here ]------------
WARNING: at drivers/ata/libahci.c:223 ahci_save_initial_config+0x20/0x268()
Modules linked in:
CPU: 1 PID: 1 Comm: swapper/0 Not tainted 3.10.53+g496fbe0 #2
[<80013b44>] (unwind_backtrace+0x0/0xf4) from [<80011544>] (show_stack+0x10/0x14)
[<80011544>] (show_stack+0x10/0x14) from [<8002c0a4>] (warn_slowpath_common+0x54/0x6c)
[<8002c0a4>] (warn_slowpath_common+0x54/0x6c) from [<8002c158>] (warn_slowpath_null+0x1c/0x24)
[<8002c158>] (warn_slowpath_null+0x1c/0x24) from [<8034c03c>] (ahci_save_initial_config+0x20/0x268)
[<8034c03c>] (ahci_save_initial_config+0x20/0x268) from [<803496b4>] (ahci_probe+0x190/0x424)
[<803496b4>] (ahci_probe+0x190/0x424) from [<80302db4>] (platform_drv_probe+0x18/0x1c)
[<80302db4>] (platform_drv_probe+0x18/0x1c) from [<80301b90>] (driver_probe_device+0x108/0x244)
[<80301b90>] (driver_probe_device+0x108/0x244) from [<8030012c>] (bus_for_each_drv+0x58/0x8c)
[<8030012c>] (bus_for_each_drv+0x58/0x8c) from [<80301a58>] (device_attach+0x74/0x88)
[<80301a58>] (device_attach+0x74/0x88) from [<80301050>] (bus_probe_device+0x84/0xa8)
[<80301050>] (bus_probe_device+0x84/0xa8) from [<2Ý68>] (device_add+0x508/0x5b8)
[<802ff768>] (device_add+0x508/0x5b8) from [<80303124>] (platform_device_add+0xb4/0x218)
[<80303124>] (platform_device_add+0xb4/0x218) from [<8034d190>] (imx_ahci_probe+0x1a0/0x200)
[<8034d190>] (imx_ahci_probe+0x1a0/0x200) from [<80302db4>] (platform_drv_probe+0x18/0x1c)
[<80302b4>] (platform_drv_probe+0x18/0x1c) from [<80301b90>] (driver_probe_device+0x108/0x244)
[<80301b90>] (driver_probe_device+0x108/0x244) from [<80301d9c>] (__driver_attach+0x8c/0x90)
[<80301d9c>] (__driver_attach+0x8c/0x90) from [<8030008c>] (bus_for_each_dev+0x60/0x94)
[<8030008c>] (bus_for_ea_dev+0x60/0x94) from [<8030133c>] (bus_add_driver+0x1c0/0x24c)
[<8030133c>] (bus_add_driver+0x1c0/0x24c) from [<80302398>] (driver_register+0x78/0xf8)
[<80302398>] (driver_register+0x78/0xf8) from [<8000871c>] (do_one_initcall+0x108/0x158)
[<8000871c>] (do_one_initcall+0x108/0x158) from [<80c09be0>] (kernel_init_freeable+0x138/0x1d8)
[<80c09be0>] (kernel_init_freeable+0x1&zÂÅd8) from [<8062e098>] (kernel_init+0x8/0x158)
[<8062e498>] (kernel_init+0x8/0x158) fom [<8000dfd8>] (ret_from_fork+0x14/0x3c)
---[ end trace e8addf7b0126f9fb ]---
ahci ahci: forcing PORTS_IMPL to 0x1
------------[ cut here ]------------
WARNING: at drivers/ata/libahci.c:223 ahci_reset_controller+0x1c/0x160()
Modules linked in:
CPU: 1 PID: 1 Comm: swapper/0 Tainted: G W 3.10.53+g496fbe0 #2
[<80013b44>] (unwind_backtrace+0x0/0xf4) from [<80011544>] (show_stack+0x10/0x14)
[<80011544>] (show_stack+0x10/0x14) from [<8002c0a4>] (warn_s
owpath_common+0x54/0x6c)
[<8002c0a4>] (warn_slowpath_common+0x54/0x6c) from [<8002c158>] (warn_slowpath_null+0x1c/0x24)
[<8002c158>] (warn_slowpath_null+0x1c/0x24) from [<8034c2a0>] (ahci_reset_controller+0x1c/0x160)
[<8034c2a0>] (ahci_reset_controller+0x1c/0x160) from [<80349808>] (ahci_probe+0x2e4/0x424)
[<80349808>] (ahci_probe+0x2e4/0x424) from [<80302db4>] (platform_drv_probe+0x18/0x1c)
[<80302db4>] (platform_drv_probe+0x18/0x1c) from [<80301b90>] (driver_probe_device+0x108/0x244)
[<80301b90>] (driver_probe_device+0x108/0x244) from [<8030012c>] (bus_for_each_drv+0x58/0x8c)
[<8030012c>] (bus_for_each_drv+0x58/0x8c) from [<80301a58>] (device_attach+0x74/0x88)
[<80301a58>] (device_attach+0x74/0x88) from [<80301050>] (bus_probe_device+0x84/0xa8)
[<80301050>] (bus_probe_device+0x84/0xa8) from [<802ff768>] (device_add+0x508/0x5b8)
[<802ff768>] (device_add+0x508/0x5b8) from [<80303124>] (platform_device_add+0xb4/0x218)
[<80303124>] (platform_device_add+0xb4/0x218) from [<8034d190>] (imx_ahci_probe+0x1a0/0x200)
[<8034d190>] (imx_ahci_probe+0x1a0/0x200) from [<80302db4>] (platform_drv_probe+0x18/0x1c)
[<80302db4>] (platform_drv_probe+0x18/0x1c) from [<80301b90>] (driver_probe_device+0x108/0x244)
[<80301b90>] (driver_probe_device+0x108/0x244) from [<80301d9c>] (__driver_attach+0x8c/0x90)
[<80301d9c>] (__driver_attach+0x8c/0x90) from [<8030008c>] (bus_for_each_dev+0x60/0x94)
[<8030008c>] (bus_for_each_dev+0x60/0x94) from [<8030133c>] (bus_add_driver+0x1c0/0x24c)
[<8030133c>] (bus_add_driver+0x1c0/0x24c) from [<80302398>] (driver_register+0x78/0xf8)
[<80302398>] (driver_register+0x78/0xf8)from [<8000871c>] (do_one_initcall+0x108/0x158)
[<8000871c>] (do_one_initcall+0x108/0x158) from [<80c09be0>] (kernel_init_freeable+0x138/0x1d8)
[<80c09be0>] (kernel_init_freeable+0x138/0x1d8) from [<8062e498>] (kernel_init+0x8/0x158)
[<8062e498>] (kernel_init#0x8/0x158) from [<8000dfd8>] (ret_from_fork+0x14/0x3c)
---[ end trace e8addf7b0126f9fc ]---
------------[ cut here ]------------
WARNING: at drivers/ata/libahci.c:223 ahci_reset_controller+0xa4/0x160()
Modules linked in:
PU: 1 PID: 1 Comm: swapper/0 Tainted: G W 3.10.53+g496fbe0 #2
[<80013b44>] (unwind_backtraca+0x0/0xf4) from [<80011544>] (show_stack+0x10/0x14)
[<80011544>] (show_stack+0x10/0x14) from [<8002c0a4>] (warn_slowpath_common+0x54/0x6c)
[<8002c0a4>] (warn_slowpath_common+0x54/0x6c) from [<8Å58>] (warn_slowpath_null+0x1c/0x24)
[<8002c158>] (warn_slowpath_null+0x1c/0x24) from [<8034c328>] (ahci_reset_controller+0xa4/0x160)
[<8034c328>] (ahci_reset_contro
ler+0xa4/0x160) from [<80349808>] (ahci_probe+0x2e4/0x424)
[<80349808>] (ahci_probe+0x2e4/0x424) from [<80302db4>] (platform_drv_probe+0x18/0x1c)
80302db4>] (platform_drv_probe+0x18/0x1c) from [<80301b90>] (driver_probe_device+0x108/0x244)
[<80301b90>] (driver_probe_device+0x108/0x244) from [<8030012c>] (bus_for_each_drv+0x58/0x8c)
[<8030012c>] (bus_for_each_drv+0x58/0x8c) from [<80301a58>] (device_attach+0x74/0x88)
[<80301a58>] (device_attach+0x74/0x88) from [<80301050>] (bus_probe_device+0x84/0xa8)
[<80301050>] (bus_probe_device+0x84/0xa8) from [<802ff768>] (device_add+0x508/0x5b8)
[<802ff768>] (device_add+0x508/0x5b8) frol [<80303124>] (platform_device_add+0xb4/0x218)
[<80303124>] (platform_device_add+0xb4/0x218) from [<8034d190>] (imx_ahci_probe+0x1a0/0x200)
[<8034d190>] (imx_ahci_probe+0x1a0/0x200) from [<80302db4>] (platform_drv_probe+0x18/0x1c)
[<80302db4>] (platform_drv_probe+0x18/0x1c) from [<80301b90>] (driver_probe_device+0x108/0x244)
[<80301b90>] (driver_probe_device+0x108/0x244) from [<80301d9c>] (__driver_attach+0x8c/0x90)
[<80301d9c>] (__driver_attach+0x8c/0x90) from [<8030008c>] (bus_for_each_dev+0x60/0x94)
[<8030008c>] (bus_for_each_dev+0x60/0x94) from [<8030133c>] (bus_add_driver+0x1c0/0x24c)
[<8030133c>] (bus_add_driver+0x1c0/0x24c) from [<80302398>] (driver_register+0x78/0xf8)
[<80302398>] (driver_register+0x78/0xf8) from [<8000871c>] (do_one_initcall+0x108/0x158)
[<8000871c>] (do_one_initcall+0x108/0x158) from [<80c09be0>] (kernel_init_freeable+0x138/0x1d8)
[<80c09be0>] (kernel_init_freeable+0x138/0x1d8) from [<8062e498>] (kernel_init+0x8/0x158)
[<8062e498>] (kernel_init+0x8/0x158) from [<8000dfd8>] (ret_from_fork+0x14/0x3c)
---[ end trace e8addf7b0126f9fd ]---
ahci ahci: AHCI 0000.0000 1 slots 1 ports ? Gbps 0x1 impl platformmode
ahci ahci: flags:
scsi0 : ahci_platform
ata1: SATA max UDMA/133 mmio [mem 0x02200000-0x02203fff] port 0x100 irq 71
m25p80 spi32766.0: unrecognized JEDEC id ffffff
spi_imx 2008000.ecspi: probed
libphy: fec_enet_mii_bus: probed
fec 2188000.ether`et eth0: registered PHC device 0
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
usbcore: registered new interface driver usb-storage
ci_hdrc ci_hdrc.1: doesn't support gadget
ci_hdrc ci_hdrc.1: EHCI Host Controller
ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1
ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
mousedev: PS/2 mouse device common for all mice
elan-touch 2-0010: elan - Read Hello Packet Failed
elan-touch: probe of 2-0010 failed with error -22
egalax_ts 1-0004: Failed to read firmware version
egalax_ts: probe of 1-0004 failed with error -5
egalax_ts 2-0004: Failed po read firmware version
egalax_ts: probe of 2-0004 failed with error -5
input: max11801_ts as /devices/soc0/soc.1/2100000.aips-bus/21a4000.i2c/i2c-1/1-0048/input/input0
i2c-core: driver [isl29023] using legacy suspend method
i2c-core: driver [isl29023] using legacy resume method
snvs_rtc 20cc034.snvs-rtc-lp: rtc core: registered 20cc034.snvs-rtc-lp as rtc0
i2c /dev entries driver
mxc_v4l2_output v4l2_out.39: V4L2 device registered as video16
mxc_v4l2_output v4l2_out.39: V4L2 device registered as video17
mxc_v4l2_output v4l2_out.39: V4L2 device registered as video18
mxc_v4l2_output v4l2_out.39: V4L2 device registered as video19
mxc_v4l2_output v4l2_out.39: V4L2 device registered as video20
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_BD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
mag3110 2-000e: check mag3110 chip ID
mag3110 2-000e: read chip ID 0xfffffffb is not equal to 0xc4!
mag3110: probe of 2-000e failed with error -22
i2c-core: driver [mag3110] using legacy suspend method
i2c-core: driver [mag3110] using legacy resume method
mma8451 0-001c: read chip ID 0x1 is not equal to 0x1a or 0x2a!
mma8451: probe of 0-001c failed with error -22
imx2-wdt 20bc000.wdog: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=0)
cpuidle: using governor ladder
cpuidle: using governor menu
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
.k¥µpltfm: SDHCI platform and OF driver helper
mmc1: no vqmmc regulator found
mmc1: no vmmc regulator found
mmc1: SDHCI controller on 2194000.usdhc [2194000.usdhc] using ADMA
mmc2: no vqmmc regulator found
mmc0: no vmmc regulator found
mmc2: SDHCI controller on 2198000.usdhc [2198000.usdhc] using ADMA
mmc3: no vqmmc regulator found
mmc3: no vmmc regulator found
mmc3: SDHCI controller on 219c000.usdhc [219c000.usdhc] using ADMA
Galcore version 5.0.11.25762
mmc2: new high speed SDHC card at address b368
mmcblk2: mmc2:b368 NCard 7.48 GiB (ro)
mmcblk2: p1 p2 p3 < p5 p6 p7 > p4
mmcblk2: p4 size 13514752 extends beyond EOD, truncated
mmc3: BKOPS_EN bit is not set
mmc3: new high speed DDR MMC card at address 0001
mmcblk3: mmc3:0001 8WMB3R 7.28 GiB
mmcblk3boot0: mmc3:0001 8WMB3R partition 1 4.00 MiB
mmcblk3boot1: mmc3:0001 8WMB3R partition 2 4.00 MiB
mmcblk3rpmb: mmc3:0001 8WMB3R partition 3 512 KiB
mmcblk3: unknown partition table
mmcblk3boot1: unknown partition table
mxc_vdoa 21e4000.vdoa: i.MX Video Data Order Adapter(VDOA) driver probed
mmcblk3boot0: unknown partition table
mxc_asrc 2034000.asrc: mxc_asrc registered
mxc_vpu 2040000.vpu: VPU initialized
ata1: failed to resume link (SControl 0)
ata1: SATA link down (SStatus 0 SControl 0)
caam 2100000.caam: Instantiated RNG4 SH0
caam 2100000.caam: Instantiated RNG4 SH1
caam 2100000.caam: device ID = 0x0a160100 (Era 4)
caam 2100000.caam: job rings = 2, qi = 0
caam algorithms registered in /proc/crypto
caam_jr 2101000.jr0: registering rng-caam
platform caam_sm: blkkey_ex: 4 keystore units available
platform caam_sm: 64-bit clear key:
platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
platform caam_sm: 64-bit black key:
platform caam_sm: [0000] e8 77 ef a2 1f c3 26 c2
platform caam_sm: [0008] 8f 47 01 7c de cc 9c cd
platform caam_sm: 128-bit clear key:
platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
platform caam_sm: [0008] 08 09 0a 0b 0c 0` 0e 0f
platform caam_sm: 128-bit black key:
platform caam_sm: [0000] 4f 9b f5 f0 df f7 df fa
platform caam_sm: [0008] d1 20 10 4e 73 12 7f a4
platform caam_sm: 192-bit clear key:
platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f
platform caam_sm: [0016]
¢
ª
²
ºj
platform caam_sm: 192-bit black key:
platform caam_sm: [0000] ee f0 ba c9 b8 b0 7e c8
platform caam_sm: [0008] 21 44 83 a3 76 03 6e b6
platform caam_sm: [0016] 93 e4 ff c8 74 75 55 48
platform caam_sm: [0024] 9f 59 92 20 49 38 1e ef
platform caam_sm: 256-bit clear key:
platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f
platform cXX[5µé [0016] 10 11 12 13 14 15 16 17
platform caam_sm: [0024] 18 19 1a 1b 1c 1d 1e 1f
platform caam_sm: 256-bit black key:
platform caam_sm: [0000] c9 08 7b af f7 b4 6e 5a
platform caam_sm: [0008] 6c be 7d 6e 03 78 21 22
platform caam_sm: [0016] 7a 5b f4 05 db 2c 75 e9
platform caam_sm: [0024] 93 d1 b5 df 78 2e cb 39
platform caam_sm: 64-bit unwritten blob:
platform caam_sm: [0000] 00 00 00 00 00 00 00 00
platform caam_sm: [0008] 00 00 00 00 00 00 00 00
platform caam_sm: [0016] 00 00 00 00 00 00 00 00
platform caam_sm: [0024] 00 00 00 00 00 00 00 00
platform caam_sm: [0032] 00 00 00 00 00 00 00 00
platform caam_sm: [0040] 00 00 00 00 00 00 00 00
platform caam_sm: [0048] 00 00 00 00 00 00 00 00
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 128-bit unwritten blob:
platform caam_sm: [0000] 00 00 00 00 00 00 00 00
p+?½Éµcaam_sm: [0008] 00 00 00 00 00 00 00 00
platform caam_sm: [0016] 00 00 00 00 00 00 00 00
platform caam_sm: [0024] 00 00 00 00 00 00 00 00
platform cam_sm: [0032] 00 00 00 00 00 00 00 00
platform caam_sm: [0040] 00 00 00 00 00 00 00 00
platform caam_sm: [0048] 00 00 00 00 00 00 00 00
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 196-bit unwritten blob:
platform caam_sm: [0000] 00 00 00 00 00 00 00 00
platform caam_sm: [0008] 00 00 00 00 00 00 00 00
platform caam_sm: [0016] 00 00 00 00 00 00 00 00
platform caam_sm: [0024] 00 00 00 00 00 00 00 00
platform `aam_sm: [0032] 00 00 00 00 00 00 00 00
platform caam_sm: [0040] 00 00 00 00 00 00 00 00
platform caam_sm: [0048] 00 00 00 00 00 00 00 00
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 256-bit unwritten blob:
platform caa[5µé [0000] 00 00 00 00 00 00 00 00
platform caam_sm: [0008] 00 00 00 00 00 00 00 00
: [0016] 00 00 00 00 00 00 00 00
platform caam_sm: [0024] 00 00 00 00 00 00 00 00
platform caam_sm: [0032] 00 00 00 00 00 00 00 00
platform caam_sm: [0040] 00 00 00 00 00 00 00 00
platform caam_sm: [0048] 00 00 00 00 00 00 00 00
platform caam_sm: [0056] 00 00 00 00 00 0 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 64-bit black key in blob:
platform caam_sm: [0000] 15 5e 51 fb a3 f5 a9 8b
platform caam_sm: [0008] 23 cd 8a 68 da 41 39 30
platform caam_sm: [0016] ae 66 39 71 79 74 20 17
platform caam_sm: [0024] 15 e8 cb b3 4a ec d6 42
platform caam_sm: [0032W
Å 29 10 2d 30 67 3b c1
platform caam_sm: [0040] 20 4c 54 ca 6c 8b b3 46
platform caam_m: [0048] 53 92 86 77 8f 27 cf 4c
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 j
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 128-bit black key in blob:
platform caam_sm: [0000] 20 88 80 6a 48 41 df 0b
platform caam_sm: [0008] 70 7b 8d e6 b6 23 94 78
plapform caam_sm: [0016] 90 78 ef aa 7f b0 57 5c
platform caam_sm: [0024] f4 4e 40 ea fa 53 f7 0c
platfopm caam_sm: [0032] 3a dd bc 4f 10 f7 5f 0b
platform caam_sm: [0040] f0 2a 60 c2 b3 fc 61 b0
platform caam_sm: [0048] 88 a3 5b 32 6e bd b4 e7
platform caam_sm: [0056] 4f 4c 06 8f 4e 0d 39 39
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 0 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 192-bit black key in blob:
platform caam_sm: [0000] ab c0 57 5f 5a 92 b1 b0
platform caam_sm: [0008] dd 32 ca c9 73 f1 df 61
platform caam_sm: [0016] 4f b2 79 a8 e2 a9 1c d2
platform caam_sm: [0024] 47 6c 9c c5 4f 1a e7 f2
platform caam_sm: [0032] c2 b3 1f 35 97 6d a2 32
platform caam_sm: [0040] ed b1 aa 86 3d a4 f8 63
plapform caam_sm: [0048] c4 3d b0 2d c9 c5 6c 0d
platform caam_sm: [0056] 05 b2 6c 62 8c 89 69 9e
platform caam_sm: [0064] e5 80 90 8f 14 23 c0 3d
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platfrm caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 256-bit black key in blob:
platform caam_sm: [0000] 5b d7 a4 f5 f1 f4 f1 ff
platform caam_sm: [0008] 43 50 de 1b bd a9 08 4e
platform caam_sm: [0016] 8b aa 21 e7 cb 9c a7 c5
platform caam_sm: [0024] ea f1 d5 68 00 33 90 94
platform caam_sm: [0032] 4b 29 af 1c 84 35 ac 03
platform caam_sm: [0040] 0d 76 7d 7b 64 f1 9e c2
platform caam_sm: [0048] fc a9 74 47 73 f0 fa e8
platform caam_sm: [0056] 99 9b 46 0d e1 0b 06 60
platform caam_sm: [0064] 92 a0 53 41 7a 88 e2 b6
platform caam_sm: [0072] 37 de d5 79 32 e3 30 b8
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: restored 64-bit black Vé
platform caam_sm: [0000] 16 08 9b 77 b6 75 32 eb
platform caam_sm: [0008] d1 20 a3 f6 ac 5b 7e a6
platform caam_sm: restored 128-bit black key:
platform caam_sm: [0000] 4f 9b f5 f0 df f7 df fa
platform caam_sm: [0008] d1 20 10 4e 73 12 7f a4
platform caam_sm: restored 192-bit black key:
platform caam_sm: [0000] ee f0 ba c9 b8 b0 7e c8
platform caam_sm: [0008] 21 44 83 a3 76 03 6e b6
platform caam_sm: [0016] 1d 80 54 96 98 8f 34 30
platform caam_sm: [0024] 45 ac cc 20 8e d7 d3 04
platform caam_sm: restored 256-bit black key:
platform caam_sm: [0000] c9 08 7b af f7 b4 6e 5a
platform ¬µ}?é [0008] 6c be 7d 6e 03 78 21 22
platform caam_sm: [0016] 7a 5b f4 05 db 2c 75 e9
platform caam_sm: [0024] 93 d1 b5 df 78 2e cb 39
snvs-secvio 20cc000.caam-snvs: violation handlers armed - non-secure state
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
wm8962 0-001a: Failed to read ID register
wm8962: probe of 0-001a failed with error -5
imx-wm8962 sound.29: failed to find codec platform device
imx-wm8962: probe of sound.29 failed with error -22
imx-audio-hdmi sound-hdmi.30: hdmi-hifi <-> hdmi_audio.17 mapping ok
TCP: cubic registered
NET: Registered protocol family 10
sit: IPv6 over IPv4 tunneling driver
NET: Registered protocol family 17
8021q: 802.1Q VLAN Support v1.8
Key type dns_resolver registered
VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
VGEN3: disabling
ÿÿÿÿW¿¹ð
You say your trying to download an Image to the eMMC, but it looks like the download process isn't starting (Linux kernel hangs).
Are you able to boot Linux with an initramfs?
Can you attach your mfg ucl2.xml ?
Hi Igor,
Thanks for your prompt reply.
1. I would like to know whether "bitbake fsl-image-mfgtool-initramfs" can apply in android project? If so, what should I export BBPATH to in order to build zImage?
2. My side haven't any ddr tester to test ddr settings of eMMC, is there any other way to guess these parameters? Which files should I modify to change these parameters?
Br,
Jackie
HI Jackie
1. yes MFG Tools images (firmware) should be rebuilt even if one uses it
for flashing android images.
2. it does not matter eMMC is used for flashing or other media, such as nand or SD.
For new board firmware should be rebuilt so new ddr settings, specific for custom board,
could be used by MFG Tool.
Best regards
igor
Hi Igor,
1. When I run "bitbake fsl-image-mfgtool-initramfs",debug message "BBPATH variable is not set" is shown, which directory should I refer to?
2. Which file save those ddr settings of eMMC?
Thanks.
BR,
Jackie
Hi Igor,
I tried to download images into SD rather than eMMC, the mfgtool firmware still stucks at "VGEN3: disabling", please kindly advise.
Galcore version 5.0.11.25762
mmc2: new high speed SDHC card at address 0001
mmcblk2: mmc2:0001 SD8GB 7.32 GiB
mmcblk2: p1 p2 p3 < p5 p6 p7 p8 > p4
Jackie
Jackie,
How about the device tree for this custom board?
Have you changed the device tree compiled dtb and put to the mfg tool.
BTW, the mfg tool for KK4.4.3_200 is android_KK4.4.3_2.0.0-ga_tools.tar.gz
And in this is easy way to double click the mfgtool2-android-mx6q-sabresd-emmc.vbs to flash the board.
Hi Jackie
just for test one can try to build linux min image and flash it
L3.10.53_1.1.0_iMX6QDLS_Bundle
~igor
Hi Jackie
if kernel hangs this may be caused by improper ddr settings, one can rebuild MFG Tools
firmware with new ddr settings specific for custom board (obtain them from ddr tester),
use sect.6.2 The Manufacturing Tool, MFGTool attached Yocto Guide.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
May be ddr setting of eMMC can't be solved within several days, I would like to use TF-card to save the image. However there isn't WP pin in TF-card, how can I disable the WP detection and build again the ram uboot and kernel for downloading *.img files. Thanks.
BR,
Jackie
mmc2: new high speed SDHC card at address b368
mmcblk2: mmc2:b368 NCard 7.48 GiB (ro)
mmcblk2: p1 p2 p3 < p5 p6 p7 > p4
mmcblk2: p4 size 13514752 extends beyond EOD, truncated