IMX6Q custom board to download *.img by using MFGTool2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6Q custom board to download *.img by using MFGTool2

2,170件の閲覧回数
ASTRIHK
Contributor III

I'm using KK4.4.3_2.0.0-ga release. This release is based on the L3.10.53 kernel. When I use MFGTool2 to download *.img into eMMC of my custom board, the download process stops after printing debug messge "VGEN3: disabling".  One of the debug message shows "mmcblk3: unknown partition table", it seems eMMC can't be partitioned. Please kindly advise. Also, based on L3.10.53 kernel version, how to build ram uboot and kernel for MFGTool2? Thanks.

U-Boot 2014.04 (Jan 05 2015 - 14:54:36)

CPU:   Freescale i.MX6Q rev1.5 at 792 MHz

CPU:   Temperature 31 C, calibration data: 0x57f4ea69

Reset cause: POR

Board: MX6-SabreSD

I2C:   ready

DRAM:  1 GiB

MMC:   FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2

No panel detected: default to Hannstar-XGA

Display: Hannstar-XGA (1024x768)

In:    serial

Out:   serial

Err:   serial

Found PFUZE100 deviceid=10,revid=21

Net:   Phy not found

PHY reset timed out

FEC [PRIME]

Boot from USB for mfgtools

Use default environment for mfgtools

Run ootcmd_mfg: run mfgtool_args;bootz ${loadaddr} ${initrd_addr} ${fdt_addr};

Hit any key to stop autoboot:  0

Kernel image @ 0x12000000 [ 0x000000 - 0x5093d0 ]

## Loading init Ramdisk from Legacy Image at 12c00000 ...

   Image Name:   fsl-image-mfgtool-initramfs-imx6

   Image Type:   ARM Linux RAMDisk Image (gzip compressed)

   Data Size:    7377681 Bytes = 7 MiB

   Load Address: 00000000

   Entry Point:  00000000

   Verifying Checksum ... OK

## Flattened Device Tree blob at 18000000

   Booting using the fdt blob a 0x18000000

   Using Device Tree in place at 18000000, end 1800f1a6

Starting kernel ...

Booting Linux on physical CPU 0x0

Linux version 3.10.53+g496fbe0 (fsl64@fsl64) (gcc version 4.8.1 (GCC) ) #2 SMP Sat Jul 4 19:16:53 CST 2015

CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d

CPU: PIPT / VHPT nonaliasing data cache, VIPT aliasing instruction cache

Machine: Freescale i.MX6 Quad/DualLite (Device Tree), model: Freescale i.MX6 Quad SABRE Smart Device Board

cma: CMA: reserved 320 MiB at 3c000000

Memory policy: ECC diabled, Data cache writealloc

PERCPU: Embedded 8 pages/cpu @81528000 s8768 r8192 d15808 u32768

Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 260096

Kernel command line: console=ttymxc0,115200 rdinit=/linuxrc g_mass_storage.stall=0 g_mass_storage.removable=1 g_mass_storage.idVendor=0x066F g_mass_storage.idProduct=0x37FF g_mass_storage.iSerialNumber= enable_wait_mode=off

PID hash table entries: 4096 (order: 2, 16384 bytes)

Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)

Inode-cache hash table entries: 5536 (order: 6, 262144 bytes)

Memory: 1024MB = 1024MB total

Memory: 690396k/690396k available, 358180k reserved, 0K highmem

Virtual kernel memory layout:

    vector  : 0xffff0000 - 0xffff1000   (   4 kB)

    fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)

    vmalloc : 0xc0800000 - 0xff000000   (1000 MB)

    lowmem  : 0x80000000 - 0xc0000000   (1024 MB)

    modules : 0x7f000000 - 0x80000000   (  16 MB)

      .text : 0x8000800 - 0x80c08604   (12290 kB)

      .init : 0x80c09000 - 0x80c5b240   ( 329 kB)

      .data : 0x80c5c000 - 0x80cad180   ( 325 kB)

       .bss : 0x80cad180 - 0x80d0f714   ( 394 kB)

SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1

Hierarchical RCU implementation.

NR_IRQS:16 nr_irqs:16 16

L310 cache controller enabled

l2x0: 16 ways, CACHE_ID 0x410000c7, AUX_CTRL 0x32070000, Cache size: 1048576 B

sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655ms

CPU identified as i.MX6Q, silicon rev 1.5

Console: colour dummy device 80x30

Calibrating delay loop... 1581.5 BogoMIPS (lpj=7905280)

pid_max: default: 3768 minimum: 301

Mount-cache hash table entries: 512

CPU: Testing write buffer coherency: ok

CPU0: thread -1, cpu 0, socket 0, mpidr 80000000

Setting up static identity map for 0x80639f00 - 0x80639f58

CPU1: Booted secondary processor

CPU1: thread -1, cpu 1, socket 0, mpidr 80000001

CPU2: Booted secondary processor

CPU2: thread -1, cpu 2, socket 0, mpidr 80000002

CPU3: Booted scondary processor

CPU3: thread -1, cpu 3, socket 0, mpidr 80000003

Brought up 4 CPUs

SMP: Total of 4 processors activated (6324.22 BogoMIPS).

CPU: All CPU(s) started in SVC mode.

devtmpfs: initialized

pinctrl core: initialized pinctrl subsystem

regulator-dummy: no parameters

NET: Registered protocol family 16

DMA: preallocated 256 KiB pool for atomic coherent allocations

Use WDOG1 as reset source

syscon 20c8000.anatop: regmap [mem 0x020c8000-0x020c8fff] registered

vdd1p1: 800 <--> 1375 mV at 1125 mV

vdd3p0: 2800 <--> 3150 mV at 3000 mV

vdd2p5: 2000 <--> 2750 mV at 2425 mV

cpu: 725 <--> 1450 mV at 1150 mV

vddpu: 725 <--> 1450 mV

vddsoc: 725 <--> 1450 mV at 1175 mV

syscon 20e0000.iomuxc-gpr: regmap [mem 0x020e0000-0x020e0037] registered

syscon 21bc000.ocotp-ctrl: regmap [mem 0x021bc000-0x021bffff] registered

hw-breakpoint: found 5 (+1 reserved) breakpoint an` 1 watchpoint registers.

hw-breakpoint: maximum watchpoint size is 4 bytes.

imx6q-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver

bio: create slab <bio-0> at 0

mxs-dma 110000.dma-apbh: initialized

usb_otg_vbus: 5000 mV

usb_h1_vbus: 5000 mV

wm8962-supply: no parameters

mipi_dsi_pwr_on: no parameters

sensor-supply: 3300 mV

i2c-core: driver [max17135] using legacy suspend method

i2c-core: driver [max17135] using legacy resume method

SCSI subsystem initialized

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

i2c i2c-0: IMX I2C adapter registered

i2c i2c-1: IMX A2C adapter registered

i2c i2c-2: IMX I2C adapter registered

Linux video capture interface: v2.00

pps_core: LinuxPPS API ver. 1 registered

pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>

PTP clock support registered

imx-ipuv3 2400000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)

imx-ipuv3 2800000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(0,5), 5F(6,7)

mxc_mipi_csi2 21dc000.mipi_csi: i.MX MIPI CSI2 driver probed

mxc_mipi_csi2 21dc000.mipi_csi: i.MX MIPI CSI2 dphy version is 0x3130302a

MIPI CSI2 driver module loaded

Advanced Linux Sound Architecture Driver Initialized.

cfg80211: Calling CRDA to update world regulatory domain

pureg-dummy: `o parameters

Switching to clocksource mxc_timer1

NET: Registered protocol family 2

TCP established hash table entries: 8192 (order: 4, 65536 bytes)

TCP bind hash table entries: 8192 (order: 4, 65536 bytes)

TCP: Hash tables configured (established 8192 bind 8192)

TCP: reno registered

UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)

NET: Regiptered protocol family 1

RPC: Registered named UNIX socket transport module.

RPC: Registerd udp transport module.

RPC: Registered tcp transport module.

RPC: Registered tcp NFSv4.1 backchannel transport module.

Trying to unpack rootfs image as initramfs...

Freeing initrd memory: 7200K (82c01000 - 83309000)

hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available

imx6_busfreq busfreq.16: DDR medium rate not supported.

Bus freq driver module loaded

futex hash table entries: 1024 (orde.'¢b²ªª²åÑ?

VFS: Disk quotas dquot_6.5.2

Dquot-cache hash table entries: 1024 (order 0, 4096 bxtes)

NFS: Registering the id_resolver key type

Key type id_resolver registered

Key type id_legacy registered

jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.

fuse init (API version 7.22)

msgmni has been set to 2002

io scheduler noop registered

io scheduler dea`line registered

io scheduler cfq registered (default)

imx-weim 21b8000.weim: WEIM driver registered.

mxc_mipi_dsi 21e0000.mipi: i.MX MIPI DSI driver probed

MIPI DSI driver module loaded

mxc_sdc_fb fb.1: registered mxc display driver ldb

imx-ipuv3 2800000.ipu: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)

Console: switching to colour frame buffer device 128x48

mxc_hdmi 20e0000.hdmi_video: Detected HDMI controller 0x13:0xa:0xa0:0xc1

fbcvt: 1920x1080@60: CVT Name - 2.073M9

mxc_sdc_fb fb.32: registered mxc display driver hdmi

mxc_sdc_fb fb.33: registered mxc display driver lcd

mxc_sdc_fb fb.33: ipu0-di0 already in use

mxc_sdc_fb: probe of fb.33 failed with error -16

mxc_sdc_fb fb.34: registered mxc display driver ldb

imx-sdma 20ec000.sdma: no iram assigned, using external mem

imx-sdma 20ec000.sdma: loaded firmware 1.1

imx-sdma 20ec000.sdma: initialized

pfuze10-regulator 1-0008: Full lay: 2, Metal lay: 1

pfuze100-regulator 1-0008: FAB: 0, FIN: 0

p`uze100-regulator 1-0008: pfuze100 found.

SW1AB: 300 <--> 1875 mV at 1375 mV

SW1C: 300 <--> 1875 mV at 1375 mV

SW2: 800 <--> 3300 mV at 3300 mV

SW3A: 400 <--> 1975 mV at 1500 mV

SW3B: 400 <--> 1975 mV at 1500 mV

SW4: 800 <--> 3300 mV at 3150 mV

SWBST: 5000 <--> 5150 mV at 5000 mV

VSNVS: 1000 <--> 3000 mV at 3000 mV

VREFDDR: 750 mV

VGEN1: 800 <--> 1550 mV at 1500 mV

VGEN2: 800 <--> 1550 mV at 1500 mV

VGEN3: 1800 <--> 3300 mV at 2800 mV

VGEN4: 1800 <--> 3300 mV at 1800 mV

VGEN5: 1800 <--> 3300 mV at 3000 mV

VGEN6: 1800 <--> 3300 mV at 3300 mV

Serial: IMX driver

2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 58) is a IMX

console [ttymxc0] enabled

serial: Freescale lpuart driver

imx sema4 driver is registered.

[drm] Initialized drm 1.1.0 20060810

[drm] Initialized vivante 1.0.0 20120216 on minor 0

brd: module loaded

loop:j½Õ±loaded

Wait for CR ACK error!

Wait for CR ACK error!

Wait for CR ACK error!

Wait for CR ACK error!

Wait for CR ACK error!

Wait for CR ACK error!

Wait for CR ACK error!

Wait for CR ACK error!

Wait for CR ACK error!

Wait for CR ACK error!

Wait for CR ACK error!

Wait for CR ACK error!

Wait for CR ACK error!

Wait for CR ACK error!

Wating for RX_PLL lock time out

------------[ cut here ]------------

WARNING: at drivers/ata/libahci.c:223 ahci_save_initial_config+0x20/0x268()

Modules linked in:

CPU: 1 PID: 1 Comm: swapper/0 Not tainted 3.10.53+g496fbe0 #2

[<80013b44>] (unwind_backtrace+0x0/0xf4) from [<80011544>] (show_stack+0x10/0x14)

[<80011544>] (show_stack+0x10/0x14) from [<8002c0a4>] (warn_slowpath_common+0x54/0x6c)

[<8002c0a4>] (warn_slowpath_common+0x54/0x6c) from [<8002c158>] (warn_slowpath_null+0x1c/0x24)

[<8002c158>] (warn_slowpath_null+0x1c/0x24) from [<8034c03c>] (ahci_save_initial_config+0x20/0x268)

[<8034c03c>] (ahci_save_initial_config+0x20/0x268) from [<803496b4>] (ahci_probe+0x190/0x424)

[<803496b4>] (ahci_probe+0x190/0x424) from [<80302db4>] (platform_drv_probe+0x18/0x1c)

[<80302db4>] (platform_drv_probe+0x18/0x1c) from [<80301b90>] (driver_probe_device+0x108/0x244)

[<80301b90>] (driver_probe_device+0x108/0x244) from [<8030012c>] (bus_for_each_drv+0x58/0x8c)

[<8030012c>] (bus_for_each_drv+0x58/0x8c) from [<80301a58>] (device_attach+0x74/0x88)

[<80301a58>] (device_attach+0x74/0x88) from [<80301050>] (bus_probe_device+0x84/0xa8)

[<80301050>] (bus_probe_device+0x84/0xa8) from [<2Ý68>] (device_add+0x508/0x5b8)

[<802ff768>] (device_add+0x508/0x5b8) from [<80303124>] (platform_device_add+0xb4/0x218)

[<80303124>] (platform_device_add+0xb4/0x218) from [<8034d190>] (imx_ahci_probe+0x1a0/0x200)

[<8034d190>] (imx_ahci_probe+0x1a0/0x200) from [<80302db4>] (platform_drv_probe+0x18/0x1c)

[<80302b4>] (platform_drv_probe+0x18/0x1c) from [<80301b90>] (driver_probe_device+0x108/0x244)

[<80301b90>] (driver_probe_device+0x108/0x244) from [<80301d9c>] (__driver_attach+0x8c/0x90)

[<80301d9c>] (__driver_attach+0x8c/0x90) from [<8030008c>] (bus_for_each_dev+0x60/0x94)

[<8030008c>] (bus_for_ea_dev+0x60/0x94) from [<8030133c>] (bus_add_driver+0x1c0/0x24c)

[<8030133c>] (bus_add_driver+0x1c0/0x24c) from [<80302398>] (driver_register+0x78/0xf8)

[<80302398>] (driver_register+0x78/0xf8) from [<8000871c>] (do_one_initcall+0x108/0x158)

[<8000871c>] (do_one_initcall+0x108/0x158) from [<80c09be0>] (kernel_init_freeable+0x138/0x1d8)

[<80c09be0>] (kernel_init_freeable+0x1&zÂÅd8) from [<8062e098>] (kernel_init+0x8/0x158)

[<8062e498>] (kernel_init+0x8/0x158) fom [<8000dfd8>] (ret_from_fork+0x14/0x3c)

---[ end trace e8addf7b0126f9fb ]---

ahci ahci: forcing PORTS_IMPL to 0x1

------------[ cut here ]------------

WARNING: at drivers/ata/libahci.c:223 ahci_reset_controller+0x1c/0x160()

Modules linked in:

CPU: 1 PID: 1 Comm: swapper/0 Tainted: G        W    3.10.53+g496fbe0 #2

[<80013b44>] (unwind_backtrace+0x0/0xf4) from [<80011544>] (show_stack+0x10/0x14)

[<80011544>] (show_stack+0x10/0x14) from [<8002c0a4>] (warn_s

                                                             owpath_common+0x54/0x6c)

[<8002c0a4>] (warn_slowpath_common+0x54/0x6c) from [<8002c158>] (warn_slowpath_null+0x1c/0x24)

[<8002c158>] (warn_slowpath_null+0x1c/0x24) from [<8034c2a0>] (ahci_reset_controller+0x1c/0x160)

[<8034c2a0>] (ahci_reset_controller+0x1c/0x160) from [<80349808>] (ahci_probe+0x2e4/0x424)

[<80349808>] (ahci_probe+0x2e4/0x424) from [<80302db4>] (platform_drv_probe+0x18/0x1c)

[<80302db4>] (platform_drv_probe+0x18/0x1c) from [<80301b90>] (driver_probe_device+0x108/0x244)

[<80301b90>] (driver_probe_device+0x108/0x244) from [<8030012c>] (bus_for_each_drv+0x58/0x8c)

[<8030012c>] (bus_for_each_drv+0x58/0x8c) from [<80301a58>] (device_attach+0x74/0x88)

[<80301a58>] (device_attach+0x74/0x88) from [<80301050>] (bus_probe_device+0x84/0xa8)

[<80301050>] (bus_probe_device+0x84/0xa8) from [<802ff768>] (device_add+0x508/0x5b8)

[<802ff768>] (device_add+0x508/0x5b8) from [<80303124>] (platform_device_add+0xb4/0x218)

[<80303124>] (platform_device_add+0xb4/0x218) from [<8034d190>] (imx_ahci_probe+0x1a0/0x200)

[<8034d190>] (imx_ahci_probe+0x1a0/0x200) from [<80302db4>] (platform_drv_probe+0x18/0x1c)

[<80302db4>] (platform_drv_probe+0x18/0x1c) from [<80301b90>] (driver_probe_device+0x108/0x244)

[<80301b90>] (driver_probe_device+0x108/0x244) from [<80301d9c>] (__driver_attach+0x8c/0x90)

[<80301d9c>] (__driver_attach+0x8c/0x90) from [<8030008c>] (bus_for_each_dev+0x60/0x94)

[<8030008c>] (bus_for_each_dev+0x60/0x94) from [<8030133c>] (bus_add_driver+0x1c0/0x24c)

[<8030133c>] (bus_add_driver+0x1c0/0x24c) from [<80302398>] (driver_register+0x78/0xf8)

[<80302398>] (driver_register+0x78/0xf8)from [<8000871c>] (do_one_initcall+0x108/0x158)

[<8000871c>] (do_one_initcall+0x108/0x158) from [<80c09be0>] (kernel_init_freeable+0x138/0x1d8)

[<80c09be0>] (kernel_init_freeable+0x138/0x1d8) from [<8062e498>] (kernel_init+0x8/0x158)

[<8062e498>] (kernel_init#0x8/0x158) from [<8000dfd8>] (ret_from_fork+0x14/0x3c)

---[ end trace e8addf7b0126f9fc ]---

------------[ cut here ]------------

WARNING: at drivers/ata/libahci.c:223 ahci_reset_controller+0xa4/0x160()

Modules linked in:

PU: 1 PID: 1 Comm: swapper/0 Tainted: G        W    3.10.53+g496fbe0 #2

[<80013b44>] (unwind_backtraca+0x0/0xf4) from [<80011544>] (show_stack+0x10/0x14)

[<80011544>] (show_stack+0x10/0x14) from [<8002c0a4>] (warn_slowpath_common+0x54/0x6c)

[<8002c0a4>] (warn_slowpath_common+0x54/0x6c) from [<8Å58>] (warn_slowpath_null+0x1c/0x24)

[<8002c158>] (warn_slowpath_null+0x1c/0x24) from [<8034c328>] (ahci_reset_controller+0xa4/0x160)

[<8034c328>] (ahci_reset_contro

                               ler+0xa4/0x160) from [<80349808>] (ahci_probe+0x2e4/0x424)

[<80349808>] (ahci_probe+0x2e4/0x424) from [<80302db4>] (platform_drv_probe+0x18/0x1c)

80302db4>] (platform_drv_probe+0x18/0x1c) from [<80301b90>] (driver_probe_device+0x108/0x244)

[<80301b90>] (driver_probe_device+0x108/0x244) from [<8030012c>] (bus_for_each_drv+0x58/0x8c)

[<8030012c>] (bus_for_each_drv+0x58/0x8c) from [<80301a58>] (device_attach+0x74/0x88)

[<80301a58>] (device_attach+0x74/0x88) from [<80301050>] (bus_probe_device+0x84/0xa8)

[<80301050>] (bus_probe_device+0x84/0xa8) from [<802ff768>] (device_add+0x508/0x5b8)

[<802ff768>] (device_add+0x508/0x5b8) frol [<80303124>] (platform_device_add+0xb4/0x218)

[<80303124>] (platform_device_add+0xb4/0x218) from [<8034d190>] (imx_ahci_probe+0x1a0/0x200)

[<8034d190>] (imx_ahci_probe+0x1a0/0x200) from [<80302db4>] (platform_drv_probe+0x18/0x1c)

[<80302db4>] (platform_drv_probe+0x18/0x1c) from [<80301b90>] (driver_probe_device+0x108/0x244)

[<80301b90>] (driver_probe_device+0x108/0x244) from [<80301d9c>] (__driver_attach+0x8c/0x90)

[<80301d9c>] (__driver_attach+0x8c/0x90) from [<8030008c>] (bus_for_each_dev+0x60/0x94)

[<8030008c>] (bus_for_each_dev+0x60/0x94) from [<8030133c>] (bus_add_driver+0x1c0/0x24c)

[<8030133c>] (bus_add_driver+0x1c0/0x24c) from [<80302398>] (driver_register+0x78/0xf8)

[<80302398>] (driver_register+0x78/0xf8) from [<8000871c>] (do_one_initcall+0x108/0x158)

[<8000871c>] (do_one_initcall+0x108/0x158) from [<80c09be0>] (kernel_init_freeable+0x138/0x1d8)

[<80c09be0>] (kernel_init_freeable+0x138/0x1d8) from [<8062e498>] (kernel_init+0x8/0x158)

[<8062e498>] (kernel_init+0x8/0x158) from [<8000dfd8>] (ret_from_fork+0x14/0x3c)

---[ end trace e8addf7b0126f9fd ]---

ahci ahci: AHCI 0000.0000 1 slots 1 ports ? Gbps 0x1 impl platformmode

ahci ahci: flags:

scsi0 : ahci_platform

ata1: SATA max UDMA/133 mmio [mem 0x02200000-0x02203fff] port 0x100 irq 71

m25p80 spi32766.0: unrecognized JEDEC id ffffff

spi_imx 2008000.ecspi: probed

libphy: fec_enet_mii_bus: probed

fec 2188000.ether`et eth0: registered PHC device 0

ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver

usbcore: registered new interface driver usb-storage

ci_hdrc ci_hdrc.1: doesn't support gadget

ci_hdrc ci_hdrc.1: EHCI Host Controller

ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1

ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00

hub 1-0:1.0: USB hub found

hub 1-0:1.0: 1 port detected

mousedev: PS/2 mouse device common for all mice

elan-touch 2-0010: elan - Read Hello Packet Failed

elan-touch: probe of 2-0010 failed with error -22

egalax_ts 1-0004: Failed to read firmware version

egalax_ts: probe of 1-0004 failed with error -5

egalax_ts 2-0004: Failed po read firmware version

egalax_ts: probe of 2-0004 failed with error -5

input: max11801_ts as /devices/soc0/soc.1/2100000.aips-bus/21a4000.i2c/i2c-1/1-0048/input/input0

i2c-core: driver [isl29023] using legacy suspend method

i2c-core: driver [isl29023] using legacy resume method

snvs_rtc 20cc034.snvs-rtc-lp: rtc core: registered 20cc034.snvs-rtc-lp as rtc0

i2c /dev entries driver

                       mxc_v4l2_output v4l2_out.39: V4L2 device registered as video16

mxc_v4l2_output v4l2_out.39: V4L2 device registered as video17

mxc_v4l2_output v4l2_out.39: V4L2 device registered as video18

mxc_v4l2_output v4l2_out.39: V4L2 device registered as video19

mxc_v4l2_output v4l2_out.39: V4L2 device registered as video20

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_BD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

mag3110 2-000e: check mag3110 chip ID

mag3110 2-000e: read chip ID 0xfffffffb is not equal to 0xc4!

mag3110: probe of 2-000e failed with error -22

i2c-core: driver [mag3110] using legacy suspend method

i2c-core: driver [mag3110] using legacy resume method

mma8451 0-001c: read chip ID 0x1 is not equal to 0x1a or 0x2a!

mma8451: probe of 0-001c failed with error -22

imx2-wdt 20bc000.wdog: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=0)

cpuidle: using governor ladder

cpuidle: using governor menu

sdhci: Secure Digital Host Controller Interface driver

sdhci: Copyright(c) Pierre Ossman

.k¥µpltfm: SDHCI platform and OF driver helper

mmc1: no vqmmc regulator found

mmc1: no vmmc regulator found

mmc1: SDHCI controller on 2194000.usdhc [2194000.usdhc] using ADMA

mmc2: no vqmmc regulator found

mmc0: no vmmc regulator found

mmc2: SDHCI controller on 2198000.usdhc [2198000.usdhc] using ADMA

mmc3: no vqmmc regulator found

mmc3: no vmmc regulator found

mmc3: SDHCI controller on 219c000.usdhc [219c000.usdhc] using ADMA

Galcore version 5.0.11.25762

mmc2: new high speed SDHC card at address b368

mmcblk2: mmc2:b368 NCard 7.48 GiB (ro)

mmcblk2: p1 p2 p3 < p5 p6 p7 > p4

mmcblk2: p4 size 13514752 extends beyond EOD, truncated

mmc3: BKOPS_EN bit is not set

mmc3: new high speed DDR MMC card at address 0001

mmcblk3: mmc3:0001 8WMB3R 7.28 GiB

mmcblk3boot0: mmc3:0001 8WMB3R partition 1 4.00 MiB

mmcblk3boot1: mmc3:0001 8WMB3R partition 2 4.00 MiB

mmcblk3rpmb: mmc3:0001 8WMB3R partition 3 512 KiB

mmcblk3: unknown partition table

mmcblk3boot1: unknown partition table

mxc_vdoa 21e4000.vdoa: i.MX Video Data Order Adapter(VDOA) driver probed

mmcblk3boot0: unknown partition table

mxc_asrc 2034000.asrc: mxc_asrc registered

mxc_vpu 2040000.vpu: VPU initialized

ata1: failed to resume link (SControl 0)

ata1: SATA link down (SStatus 0 SControl 0)

caam 2100000.caam: Instantiated RNG4 SH0

caam 2100000.caam: Instantiated RNG4 SH1

caam 2100000.caam: device ID = 0x0a160100 (Era 4)

caam 2100000.caam: job rings = 2, qi = 0

caam algorithms registered in /proc/crypto

caam_jr 2101000.jr0: registering rng-caam

platform caam_sm: blkkey_ex: 4 keystore units available

platform caam_sm: 64-bit clear key:

platform caam_sm: [0000] 00 01 02 03 04 0f 06 07

platform caam_sm: 64-bit black key:

platform caam_sm: [0000] e8 77 ef a2 1f c3 26 c2

platform caam_sm: [0008] 8f 47 01 7c de cc 9c cd

platform caam_sm: 128-bit clear key:

platform caam_sm: [0000] 00 01 02 03 04 0f 06 07

platform caam_sm: [0008] 08 09 0a 0b 0c 0` 0e 0f

platform caam_sm: 128-bit black key:

platform caam_sm: [0000] 4f 9b f5 f0 df f7 df fa

platform caam_sm: [0008] d1 20 10 4e 73 12 7f a4

platform caam_sm: 192-bit clear key:

platform caam_sm: [0000] 00 01 02 03 04 0f 06 07

platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f

platform caam_sm: [0016]

                        ¢

                         ª

                          ²

                           ºj

                             platform caam_sm: 192-bit black key:

platform caam_sm: [0000] ee f0 ba c9 b8 b0 7e c8

platform caam_sm: [0008] 21 44 83 a3 76 03 6e b6

platform caam_sm: [0016] 93 e4 ff c8 74 75 55 48

platform caam_sm: [0024] 9f 59 92 20 49 38 1e ef

platform caam_sm: 256-bit clear key:

platform caam_sm: [0000] 00 01 02 03 04 0f 06 07

platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f

platform cXX[5µé [0016] 10 11 12 13 14 15 16 17

platform caam_sm: [0024] 18 19 1a 1b 1c 1d 1e 1f

platform caam_sm: 256-bit black key:

platform caam_sm: [0000] c9 08 7b af f7 b4 6e 5a

platform caam_sm: [0008] 6c be 7d 6e 03 78 21 22

platform caam_sm: [0016] 7a 5b f4 05 db 2c 75 e9

platform caam_sm: [0024] 93 d1 b5 df 78 2e cb 39

platform caam_sm: 64-bit unwritten blob:

platform caam_sm: [0000] 00 00 00 00 00 00 00 00

platform caam_sm: [0008] 00 00 00 00 00 00 00 00

platform caam_sm: [0016] 00 00 00 00 00 00 00 00

platform caam_sm: [0024] 00 00 00 00 00 00 00 00

platform caam_sm: [0032] 00 00 00 00 00 00 00 00

platform caam_sm: [0040] 00 00 00 00 00 00 00 00

platform caam_sm: [0048] 00 00 00 00 00 00 00 00

platform caam_sm: [0056] 00 00 00 00 00 00 00 00

platform caam_sm: [0064] 00 00 00 00 00 00 00 00

platform caam_sm: [0072] 00 00 00 00 00 00 00 00

platform caam_sm: [0080] 00 00 00 00 00 00 00 00

platform caam_sm: [0088] 00 00 00 00 00 00 00 00

platform caam_sm: 128-bit unwritten blob:

platform caam_sm: [0000] 00 00 00 00 00 00 00 00

p+?½Éµcaam_sm: [0008] 00 00 00 00 00 00 00 00

platform caam_sm: [0016] 00 00 00 00 00 00 00 00

platform caam_sm: [0024] 00 00 00 00 00 00 00 00

platform cam_sm: [0032] 00 00 00 00 00 00 00 00

platform caam_sm: [0040] 00 00 00 00 00 00 00 00

platform caam_sm: [0048] 00 00 00 00 00 00 00 00

platform caam_sm: [0056] 00 00 00 00 00 00 00 00

platform caam_sm: [0064] 00 00 00 00 00 00 00 00

platform caam_sm: [0072] 00 00 00 00 00 00 00 00

platform caam_sm: [0080] 00 00 00 00 00 00 00 00

platform caam_sm: [0088] 00 00 00 00 00 00 00 00

platform caam_sm: 196-bit unwritten blob:

platform caam_sm: [0000] 00 00 00 00 00 00 00 00

platform caam_sm: [0008] 00 00 00 00 00 00 00 00

platform caam_sm: [0016] 00 00 00 00 00 00 00 00

platform caam_sm: [0024] 00 00 00 00 00 00 00 00

platform `aam_sm: [0032] 00 00 00 00 00 00 00 00

platform caam_sm: [0040] 00 00 00 00 00 00 00 00

platform caam_sm: [0048] 00 00 00 00 00 00 00 00

platform caam_sm: [0056] 00 00 00 00 00 00 00 00

platform caam_sm: [0064] 00 00 00 00 00 00 00 00

platform caam_sm: [0072] 00 00 00 00 00 00 00 00

platform caam_sm: [0080] 00 00 00 00 00 00 00 00

platform caam_sm: [0088] 00 00 00 00 00 00 00 00

platform caam_sm: 256-bit unwritten blob:

platform caa[5µé [0000] 00 00 00 00 00 00 00 00

platform caam_sm: [0008] 00 00 00 00 00 00 00 00

: [0016] 00 00 00 00 00 00 00 00

platform caam_sm: [0024] 00 00 00 00 00 00 00 00

platform caam_sm: [0032] 00 00 00 00 00 00 00 00

platform caam_sm: [0040] 00 00 00 00 00 00 00 00

platform caam_sm: [0048] 00 00 00 00 00 00 00 00

platform caam_sm: [0056] 00 00 00 00 00 0 00 00

platform caam_sm: [0064] 00 00 00 00 00 00 00 00

platform caam_sm: [0072] 00 00 00 00 00 00 00 00

platform caam_sm: [0080] 00 00 00 00 00 00 00 00

platform caam_sm: [0088] 00 00 00 00 00 00 00 00

platform caam_sm: 64-bit black key in blob:

platform caam_sm: [0000] 15 5e 51 fb a3 f5 a9 8b

platform caam_sm: [0008] 23 cd 8a 68 da 41 39 30

platform caam_sm: [0016] ae 66 39 71 79 74 20 17

platform caam_sm: [0024] 15 e8 cb b3 4a ec d6 42

platform caam_sm: [0032W

                        Å 29 10 2d 30 67 3b c1

platform caam_sm: [0040] 20 4c 54 ca 6c 8b b3 46

platform caam_m: [0048] 53 92 86 77 8f 27 cf 4c

platform caam_sm: [0056] 00 00 00 00 00 00 00 00

platform caam_sm: [0064] 00 00 00 00 00 j

                                         platform caam_sm: [0072] 00 00 00 00 00 00 00 00

platform caam_sm: [0080] 00 00 00 00 00 00 00 00

platform caam_sm: [0088] 00 00 00 00 00 00 00 00

platform caam_sm: 128-bit black key in blob:

platform caam_sm: [0000] 20 88 80 6a 48 41 df 0b

platform caam_sm: [0008] 70 7b 8d e6 b6 23 94 78

plapform caam_sm: [0016] 90 78 ef aa 7f b0 57 5c

platform caam_sm: [0024] f4 4e 40 ea fa 53 f7 0c

platfopm caam_sm: [0032] 3a dd bc 4f 10 f7 5f 0b

platform caam_sm: [0040] f0 2a 60 c2 b3 fc 61 b0

platform caam_sm: [0048] 88 a3 5b 32 6e bd b4 e7

platform caam_sm: [0056] 4f 4c 06 8f 4e 0d 39 39

platform caam_sm: [0064] 00 00 00 00 00 00 00 00

platform caam_sm: [0072] 00 00 00 00 00 00 00 00

platform caam_sm: [0080] 0 00 00 00 00 00 00 00

platform caam_sm: [0088] 00 00 00 00 00 00 00 00

platform caam_sm: 192-bit black key in blob:

platform caam_sm: [0000] ab c0 57 5f 5a 92 b1 b0

platform caam_sm: [0008] dd 32 ca c9 73 f1 df 61

platform caam_sm: [0016] 4f b2 79 a8 e2 a9 1c d2

platform caam_sm: [0024] 47 6c 9c c5 4f 1a e7 f2

platform caam_sm: [0032] c2 b3 1f 35 97 6d a2 32

platform caam_sm: [0040] ed b1 aa 86 3d a4 f8 63

plapform caam_sm: [0048] c4 3d b0 2d c9 c5 6c 0d

platform caam_sm: [0056] 05 b2 6c 62 8c 89 69 9e

platform caam_sm: [0064] e5 80 90 8f 14 23 c0 3d

platform caam_sm: [0072] 00 00 00 00 00 00 00 00

platform caam_sm: [0080] 00 00 00 00 00 00 00 00

platfrm caam_sm: [0088] 00 00 00 00 00 00 00 00

platform caam_sm: 256-bit black key in blob:

platform caam_sm: [0000] 5b d7 a4 f5 f1 f4 f1 ff

platform caam_sm: [0008] 43 50 de 1b bd a9 08 4e

platform caam_sm: [0016] 8b aa 21 e7 cb 9c a7 c5

platform caam_sm: [0024] ea f1 d5 68 00 33 90 94

platform caam_sm: [0032] 4b 29 af 1c 84 35 ac 03

platform caam_sm: [0040] 0d 76 7d 7b 64 f1 9e c2

platform caam_sm: [0048] fc a9 74 47 73 f0 fa e8

platform caam_sm: [0056] 99 9b 46 0d e1 0b 06 60

platform caam_sm: [0064] 92 a0 53 41 7a 88 e2 b6

platform caam_sm: [0072] 37 de d5 79 32 e3 30 b8

platform caam_sm: [0080] 00 00 00 00 00 00 00 00

platform caam_sm: [0088] 00 00 00 00 00 00 00 00

platform caam_sm: restored 64-bit black ­Vé

platform caam_sm: [0000] 16 08 9b 77 b6 75 32 eb

platform caam_sm: [0008] d1 20 a3 f6 ac 5b 7e a6

platform caam_sm: restored 128-bit black key:

platform caam_sm: [0000] 4f 9b f5 f0 df f7 df fa

platform caam_sm: [0008] d1 20 10 4e 73 12 7f a4

platform caam_sm: restored 192-bit black key:

platform caam_sm: [0000] ee f0 ba c9 b8 b0 7e c8

platform caam_sm: [0008] 21 44 83 a3 76 03 6e b6

platform caam_sm: [0016] 1d 80 54 96 98 8f 34 30

platform caam_sm: [0024] 45 ac cc 20 8e d7 d3 04

platform caam_sm: restored 256-bit black key:

platform caam_sm: [0000] c9 08 7b af f7 b4 6e 5a

platform ¬µ}?é [0008] 6c be 7d 6e 03 78 21 22

platform caam_sm: [0016] 7a 5b f4 05 db 2c 75 e9

platform caam_sm: [0024] 93 d1 b5 df 78 2e cb 39

snvs-secvio 20cc000.caam-snvs: violation handlers armed - non-secure state

usbcore: registered new interface driver usbhid

usbhid: USB HID core driver

wm8962 0-001a: Failed to read ID register

wm8962: probe of 0-001a failed with error -5

imx-wm8962 sound.29: failed to find codec platform device

imx-wm8962: probe of sound.29 failed with error -22

imx-audio-hdmi sound-hdmi.30:  hdmi-hifi <-> hdmi_audio.17 mapping ok

TCP: cubic registered

NET: Registered protocol family 10

sit: IPv6 over IPv4 tunneling driver

NET: Registered protocol family 17

8021q: 802.1Q VLAN Support v1.8

Key type dns_resolver registered

VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4

VGEN3: disabling

ÿÿÿÿW¿¹ð

ラベル(1)
0 件の賞賛
15 返答(返信)

1,393件の閲覧回数
erezsteinberg
Contributor IV

You say your trying to download an Image to the eMMC, but it looks like the download process isn't starting (Linux kernel hangs).

Are you able to boot Linux with an initramfs?

Can you attach your mfg ucl2.xml ?

0 件の賞賛

1,393件の閲覧回数
ASTRIHK
Contributor III

Yes, the kernel seems hangs. I'm unable to boot Linux with initramfs. Actually eMMC of SABRESD reference board is EOL, my hardware engineer changed SAMSUNG eMMC, he said the parameters of this eMMC are similar to reference board's.

0 件の賞賛

1,393件の閲覧回数
erezsteinberg
Contributor IV

You can't write firmware to eMMC without booting Linux first using an INITRAMFS. ....

0 件の賞賛

1,393件の閲覧回数
ASTRIHK
Contributor III

Hi Igor,

One of community member told me to build a zImage for downloading and replace this file in mfgtools\Profiles\Linux\OS Firmware\firmware , is it correct?

BR,

Jackie

0 件の賞賛

1,393件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

HI Jackie

yes correct, images are rebuilt with recipe given in Yocto Guide :

To build a manufacturing image do the following -

$ bitbake fsl-image-mfgtool-initramfs

Best regards

igor

1,393件の閲覧回数
ASTRIHK
Contributor III

Hi Igor,

Thanks for your prompt reply.

1. I would like to know whether "bitbake fsl-image-mfgtool-initramfs" can apply in android project?  If so, what should I export BBPATH to in order to build zImage?

2. My side haven't any ddr tester to test ddr settings of eMMC, is there any other way to guess these parameters? Which files should I modify to change these parameters?

Br,

Jackie

0 件の賞賛

1,393件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

HI Jackie

1. yes MFG Tools images (firmware) should be rebuilt even if one uses it

for flashing android images.

2. it does not matter eMMC is used for flashing or other media, such as nand or SD.

For new board firmware should be rebuilt so new ddr settings, specific for custom board,

could be used by MFG Tool.

Best regards

igor

0 件の賞賛

1,393件の閲覧回数
ASTRIHK
Contributor III

Hi Igor,

1. When I run "bitbake fsl-image-mfgtool-initramfs",debug message "BBPATH variable is not set" is shown, which directory should I refer to?

2. Which file save those ddr settings of eMMC?

Thanks.

BR,

Jackie

0 件の賞賛

1,393件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

HI Jackie

1.suggest to create new thread

2. file with ddr memory settings is uboot/../freescale/mx6sabresd/mx6dl_4x_mt41j128.cfg,

there is no file for "those ddr settings of eMMC"

Best regards

igor

0 件の賞賛

1,393件の閲覧回数
ASTRIHK
Contributor III

Hi Igor,

I tried to download images into SD rather than eMMC, the mfgtool firmware still stucks at "VGEN3: disabling", please kindly advise.

Galcore version 5.0.11.25762

mmc2: new high speed SDHC card at address 0001

mmcblk2: mmc2:0001 SD8GB 7.32 GiB

mmcblk2: p1 p2 p3 < p5 p6 p7 p8 > p4

Jackie

0 件の賞賛

1,392件の閲覧回数
BiyongSUN
NXP Employee
NXP Employee

Jackie,

How about the device tree for this custom board?

Have you changed  the device tree compiled dtb and put to the mfg tool.

BTW, the mfg tool for KK4.4.3_200 is android_KK4.4.3_2.0.0-ga_tools.tar.gz

And in this is easy way to double click the mfgtool2-android-mx6q-sabresd-emmc.vbs to flash the board.

0 件の賞賛

1,393件の閲覧回数
ASTRIHK
Contributor III

I have overwritten the original dtb by my compiled dtb into mfg tool folder but nothing changed on the debug print.

0 件の賞賛

1,393件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Jackie

just for test one can try to build linux min image and flash it

L3.10.53_1.1.0_iMX6QDLS_Bundle

~igor

0 件の賞賛

1,393件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Jackie

if kernel hangs this may be caused by improper ddr settings, one can rebuild MFG Tools

firmware with new ddr settings specific for custom board (obtain them from ddr tester),

use sect.6.2 The Manufacturing Tool, MFGTool attached Yocto Guide.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛

1,393件の閲覧回数
ASTRIHK
Contributor III

Hi Igor,

May be ddr setting of eMMC can't be solved within several days, I would like to use TF-card to save the image. However there isn't WP pin in TF-card, how can I disable the WP detection and build again the ram uboot and kernel for downloading *.img files. Thanks.

BR,

Jackie

mmc2: new high speed SDHC card at address b368

mmcblk2: mmc2:b368 NCard 7.48 GiB (ro)

mmcblk2: p1 p2 p3 < p5 p6 p7 > p4

mmcblk2: p4 size 13514752 extends beyond EOD, truncated

0 件の賞賛