Hello,
The SabreSD EVK MMC1 detects card as SDIO 3.0 with 4.9.11 linux-imx kernel as expected with DTS 1.8V patch taken from Igor's suggestion here. Card is a WIFI NIC.
But with later kernels like 4.14.98 and 5.10.35, the EVK doesn't detect the card as SDIO 3.0 (200MHz/1.8V), but SDIO 2.0 (50MHz/3.3V) only.
I might've missed some configuration option or something else. Please help me resolve this.
Thanks.
Hi @chetanks,
I doubt that dts and kernel configuration are compatible comparing 4.x and 5.x kernels.
Have you tried to align both the dts and the defconfig to the default ones provided with the BSP you are using?
Thank you
Marco
Hi @chetanks,
just wondering whether you had any chance of reviewing the dts as suggested.
Please let me know whether you need additional information.
Thank you
Marco