Hi,
I want to install UBUNTU14.04 or ubuntu16.04 on the IMX6Q SABRE Board for Smart Devices.
Who can help me,please. I try to install Ubuntu14.04 on SD card success .But can not flash it to emmc.
So who can give me a prompt,thank you very much.!!
我需要在 IMX6Q SABRE Board for Smart Devices的emmc上安装ubuntu14.04或者ubuntu16.04,谁能帮助我,我试着在SD卡上安装了ubuntu14.04,但是我需要把ubuntu14.04安装在emmc上,请教谁能给我个提示或者镜像,非常感谢!!!
Hi yang
please check link below
https://boundarydevices.com/tag/ubuntu/
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thank you
I am a beginner study embedded linux on a IMX6Q SABRE board.
May I ask you some question.
If I want to write system to burn into the emmc, was that first dd the uboot in SD card to run, then only use "ums 0 mmc 0" to flash the ubuntu image to emmc???
Hi jive
Thank you
I just use the mfgtool to program the images to emmc.
first I follow the https://eewiki.net/display/linuxonarm/i.MX6qSABREBoardforSmart+Devices#i.MX6qSABREBoardforSmartDevices-Availability
instruction to install the ubuntu14.04 to SD card,and it can power on success.
But I need to install ubuntu14.04 on the emmc on board.
I change the ucl2.xml in the Mfgtool,and change the (dd or tar xf)according to the tutorial above.
Then it can burn the ubuntu in emmc.But cannot restart success,error follow:
U-Boot 2014.10-dirty (Aug 23 2016 - 15:26:34)
CPU: Freescale i.MX6Q rev1.5 at 792 MHz
Reset cause: POR
Board: MX6-SabreSD
I2C: ready
DRAM: 1 GiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
MMC: no card present
MMC init failed
Using default environment
No panel detected: default to Hannstar-XGA
Display: Hannstar-XGA (1024x768)
In: serial
Out: serial
Err: serial
PMIC: PFUZE100 ID=0x10
Net: FEC
Error: FEC address not set.
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc2(part 0) is current device
SD/MMC found on device 2
Checking for: /uEnv.txt ...
Checking for: /boot/uEnv.txt ...
Invalid partition 2 **
Invalid partition 3 **
Invalid partition 4 **
Invalid partition 5 **
Invalid partition 6 **
Invalid partition 7 **
MMC: no card present
SD/MMC found on device 0
Checking for: /uEnv.txt ...
MMC: no card present
Bad device mmc 0 **
Checking for: /boot/uEnv.txt ...
MMC: no card present
Bad device mmc 0 **
MMC: no card present
Bad device mmc 0 **
MMC: no card present
Bad device mmc 0 **
MMC: no card present
Bad device mmc 0 **
MMC: no card present
Bad device mmc 0 **
MMC: no card present
Bad device mmc 0 **
MMC: no card present
Bad device mmc 0 **
=>
May you help me ? or give some tips.thank you .
jiaoyang@idriverplus.com
Thank you your help,
LIST name="ubuntu-SabreSD-eMMC" is my modify according to the
https://eewiki.net/display/linuxonarm/i.MX6qSABREBoardforSmart+Devices#i.MX6qSABREBoardforSmartDevices-Bootloader:U-Boot
instruction.
附件是我修改过的ucl2.xml,谢谢
Seems that the problem is in the uEnv.txt. So, you can modify the uEnv.txt. Please check the number behind the 'mmcblk' is setup correctly. In our BSP for the SabreSD board, mmcblk2 is SD card and mmcblk3 is EMMC. Or you can type the bootcmd in u-boot by yourself. You can read our BSP user's guide for reference. You can download the Linux BSP documentation from here :
i.MX 6 Series Software and Development Tool|NXP
For example:
There is i.MX_Linux_User's_Guide.pdf , Section 4.4.1.2 Using eMMC.
In the step 10, there is an example of bootcmd:
10. Boot up the system through RFS in eMMC by HDMI:
• For i.MX 6 boards:
U-Boot > setenv mmcargs 'setenv bootargs ${bootargs} root=/dev/mmcblk3p2 rootwait rw video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24'
use the Mfgtool-Rel-13.01.00
First the mfgtool can flash the ubuntu12.04(oneiric linaro)in emmc.
I modify the ucl2.xml to flash the Ubuntu14.04.
follow the https://eewiki.net/display/linuxonarm/i.MX6qSABREBoardforSmart+Devices#i.MX6qSABREBoardforSmartDevices-Availability instruction.