IMX6DQ firmware

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX6DQ firmware

601 次查看
khaledali
Contributor III

I want to know if IMX6DQ series have the same firmware code which is  on the ROM chip ?
and
Is it an open source firmware that i can read and modify ?
and
If yes can anyone give me a link to read from ? !

标签 (1)
0 项奖励
3 回复数

453 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Khaled

ROM sources are not open source and can not be changed,

also sources are not available for customers, sorry.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

453 次查看
khaledali
Contributor III

Ok is there any way to put any other firmware on the ROM chip ?

0 项奖励

453 次查看
igorpadykov
NXP Employee
NXP Employee

no, as ROM is one time programmable memory.

~igor