IPU Warning - IPU_INT_STAT_10 = 0x00080000
DI0 Synchronous display error interrupt
This bit indicates on the interrupt that is a result of an error during access to a synchronous display via DI0
IPU Warning - IPU_INT_STAT_5 = 0x00800000
New Frame before end-of-frame error indication of Channel interrupt. This bit is the status bit of New
Frame before end-of-frame error interrupt of Channel #n.
n Indicates the corresponding DMA channel number.
0 Interrupt is cleared.
1 Interrupt is requested.
however,i cannot decice what leads to this warning.can anyone help to tell me what config maybe connected with this warning???
Please refer to the following.
What does imx-ipuv3 imx-ipuv3.0: IPU Warning - IPU_INT_STAT_10 mean?
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
well,i see there has a patch for the IPU_INT_STAT_5 = 0x00800000,does it suit my problem?
by the way ,we have usb and ethernet/bt/wifi, have no camera.
at the same time,the BT and wifi ethernet is no connect with ipu, how can that affect my display moudle?????
You may find demo images (.sdcard fime extention), such as
" fsl-image-gui-x11-imx6qdlsolo.sdcard" for the recent BSP (L3.14.28)
in the following bundle.
http://www.freescale.com/webapp/Download?colCode=L3.14.28_1.0.0_iMX6QDLS_BUNDLE
Please use the next Linux command to copy it to SD card :
$ sudo dd if= ./fsl-image-qt5-x11-imx6qdlsolo.sdcard of=/dev/sdb bs=1M
Dear yuri,I the bsp download always fail,i will try again,
but something confuse me:
our project use mfg tool to download,i want to know what the relationship of boot.img and BSP?
in fact,maybe we have different called about bsp. can you tell me what the meaning of your meaning about BSP?