IMX6DL can support 1080P60 LVDS1 and no HD display LVDS2 simultaneously?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX6DL can support 1080P60 LVDS1 and no HD display LVDS2 simultaneously?

717 次查看
songyonglai
Contributor II

Hi everyone:

   I want to two LVDS display , LVDS1 is 1080P60 output ,and LVDS2 is no HD output ,such as 1024*768, does the IMX6DL support?  thanks very much 。

标签 (1)
0 项奖励
3 回复数

554 次查看
songyonglai
Contributor II

Hi  igorpadykov

   Thanks very much for your reply。so it can support one hdmi output and one lvds output  at the same time ? such as 1080P60 HDMI output and 1366*768 LVDS output, thanks very much。

0 项奖励

554 次查看
igorpadykov
NXP Employee
NXP Employee

yes it is supported, more details can be found in presentation

A Deep Dive into Image Processing for i.MX 6 Series Applications Processors 

Best regards
igor

0 项奖励

554 次查看
igorpadykov
NXP Employee
NXP Employee

Hi song

I am afraid not, please check performance characteristics on

sect.40.4.1 Input Parallel Display Ports i.MX6SDL Reference Manual

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SDLRM.pdf

"For dual input data interface case: Up to 85 MHz per interface. (WXGA 1366x768 @
60 frames per second, 35% blanking)."

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励