IMX6DL: How to do LCD calibration ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6DL: How to do LCD calibration ?

1,844 Views
robinsingh
Contributor III

Hi All

The red colour on my LCD is little off, it does not exactly looks like perfect red. So i want to calibrate this LCD. And i am looking for the suggestion to do that: 

here is gamma correction steps, i already tried and did not get the good result 

Gamma correction on i.MX6 

ipu-examples release notes - v0.1 

ipu-examples/framebuffer_ex1.c at master · rogeriorps/ipu-examples · GitHub 

Tried above gamma correction sample code but LCD calibration  become more bad.

here is my  platform and  setting for LVDS interface :[ Android 4.4  kernel 3.10 ]

LCD panel uses (HX8282 -Source driver / HX8696 -Gate Driver)    ---SPI interface is not out from the Panel for control so i can not set the panel registers. 

====(drivers/video/mxc/mxc_lcdif.c)===================================

static struct fb_videomode lcdif_modedb[] = {                                  

{
/* lcd 1024x600 @ 60 Hz , pixel clk @ 66MHz */
"HiMAX-WSVGA", 60, 1024, 600, 25000 , 155, 160, 8, 23, 4, 4,
FB_SYNC_CLK_LAT_FALL,
FB_VMODE_NONINTERLACED,
0,},

};

===( DTS file ) ===========:

mxcfb1: fb@0 {
compatible = "fsl,mxc_sdc_fb";
disp_dev = "ldb";
interface_pix_fmt = "RGB24";
default_bpp = <24>;/*<24>;*/
int_clk = <0>;
late_init = <0>;
status = "okay";
};

================================================================

Questions : 

1) I used the ipu example code for gamma correction, where Gout array is :

int gout[16] = {0,2,4,8,16,32,64,96,128,160,192,224,255,255,255,255};  this setting do not have any impact on my LCD color, is there any other gout value for my processor imx6dl , which i need to use or How will i calculate these value , any suggestion ?

2) Reference manual section: 38.4.9.6 Gamma correction says" Required gamma correction slope for a specific panel/display should be provided by the display manufacturer "  , can you point me,   what will be  the value i  will be suing  from gamma slope in the sample code ? 

3) Regarding Data format,    My LCD support RGB stripe(LCD document does not provide good details about this), And "RGB24" is working for me with reasonable  result.  Android HAL is using HAL_PIXEL_FORMAT_RGB_565 . is there anything i need to look from this perspective, In terms of IPU Color space conversion ? 

4) Any other pointer or reference for LCD panel calibration ?  

  

Thanks

Robin Singh

Labels (4)
0 Kudos
2 Replies

1,051 Views
igorpadykov
NXP Employee
NXP Employee

Hi Robin

one can try to use yuv viewer tool to show the YcbCr & Y’Cb’Cr image to

get an intuitive color change perception. Gamma correction slope for a specific

panel/display should be provided by the display manufacturer, one can try to

change koefficients experimentally to see effect and imitate it on PC computer.

Also one can try hue control (implemented by mixing the Cb and Cr data)
using formula provided on

http://www.google.ch/patents/US20040021671
https://en.wikipedia.org/wiki/Hue

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

1,051 Views
vikaspatil
Senior Contributor I

Hi Robin,

Looking for the same solution for custom target based on i.MX6Dualite. Have you achieved it? Could you share your finding and solutions if possible?

Thanks & Regards,

Vikash

0 Kudos