Hi,
We have got imx6D (Dual) board which is based on reference designs of Wandboard. Now, we would like to compile linux source and put Image to SD card(/boot/uImage). We are compiling linux source by:
export CC=`pwd`/gcc-linaro-arm-linux-gnueabihf-4.9-2014.09_linux/bin/arm-linux-gnueabihf-
make ARCH=arm CROSS_COMPILE=${CC} distclean
make ARCH=arm CROSS_COMPILE=${CC} wandboard_defconfig
make ARCH=arm CROSS_COMPILE=${CC}
After successful compilation, we are deploying zImage, rootfs, modules, firmware etc. and also copied respective dtb file to (/media/rootfs/boot /dtbs/{$uname-r}/
and using uEnv.txt (/media/rootfs/boot/) to pass kernel parameters . Now the board completing u-boot and coming to
"starting Kernel and it is stucking there itself.
I have following Queries:
1. Since our board IMX6D which dts files i should take as reference to generate dtb (either imx6q or imx6dl).
2. Our memory technolgy is not DDR3 but it is LPDDR2. We have modified u-boot accordingly. But will it effect kernel stage also.
3. is there any other factors, which may be causing our board not to boot completely.
Please find the dts files we are using to generate dtb file.
Original Attachment has been moved to: imx6qdl.dtsi.zip
Original Attachment has been moved to: imx6q.dtsi.zip
Original Attachment has been moved to: imx6q-wandboard.dtb.zip
Original Attachment has been moved to: imx6q-wandboard.dts.zip
Original Attachment has been moved to: imx6qdl-wandboard.dtsi.zip
Hi,
Iam not trying with Robert Nelson's linux. I already tried and it is working fine.
Now Iam trying with Linux3.10.53 with Ubuntu-Core-14.04.2-Core-armhf
with which iam facing problems like "starting kernel" and stucking there itself.
U-boot we ahve modified as per lpddr2. uboot is working now.
But may be issue with parameters passed by u-bbot to kernel and dtb file.
"How to verify the parameters passed by u-boot to kernel"
Hi,
We have tested our board with Robert Nelson's post (https://eewiki.net/display/linuxonarm/Wandboard). It is working fine (very well)
1. Modified U-boot as per our memory (LPDDR2, 400MHz and 512 MB)
2. We have used Robert's Rootfs and kernel and DTBS
(With this our board as well as Wandboard (Referenec board) both are working well)
We have developed applications and run also. it is working fine
But we would like test Linux 3.10.53 downloaded from (github wandbaord .org).
1. We have compiled it and got zImage
2. Downloaded rootfs (ubuntu-core-14.02-core-armhf
With this reference board is booting with no issues (Wandboard), But our customized board is stucking at "starting kernel"
What mistake we are doing????
for Robert Nelson's linux distribution suggest to post on its blog
actually every board has own machine maintainer, for its support
please refer to below link
Machine Maintainers
FSL Community BSP Release Notes 1.8 documentation
~igor
Hi Srinivasa
1. reference should be imx6q, also set in kernel boot line maxcpus=2
2,3. in kernel pay attention to suspend-imx6.S and recommendations given in
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------