Hi,
The problem on the imx6q android4.2.2 and kernel 3.0.35.
The same video can be played with omxplayer (not stagefright).
The following is part of the log:
01-02 08:12:00.160 V/AwesomePlayer( 2238): MEDIA_ERROR -1007
01-02 08:12:00.160 V/MediaPlayerService( 2238): [3] notify (0x4221e6a8, 100, 1, -1007)
01-02 08:12:00.160 V/SurfaceTextureClient( 2610): SurfaceTextureClient::query
01-02 08:12:00.160 V/SimpleSoftOMXComponent( 2238): msgType = 2
01-02 08:12:00.160 V/AudioSystem( 3316): ioConfigChanged() event 0
01-02 08:12:00.160 V/AudioSink( 2238): stop
01-02 08:12:00.160 V/AudioTrack( 2238): stop 0x4221fe98
01-02 08:12:00.160 E/MediaPlayer( 3316): error (1, -1007)
Thanks.
Actually, this is the effect of some memory segmentation issue of the 3.0.35 kernel. Migrating to later BSP with later kernel revision should fix the issue.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
I use GM player(imx6 default player) play the same video not problem.But I need use stagefright player.