IMX6 sabresd: mmcblk0 instead of mmcblk2 for SD3

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

IMX6 sabresd: mmcblk0 instead of mmcblk2 for SD3

跳至解决方案
1,001 次查看
maks
Contributor I

Hello all.

I was provided with custom Linux 3.18 kernel. It is not BSP. I could not make it to boot until i changed mmcroot from mmcblk2p2 to mmcblk0p2. However, from user's guide "The SD3 slot uses mmcblk2 on i.MX 6". Is this because of non BSP kernel? Could not find any information to confirm this. I am sorry, just started embedded development.

标签 (2)
0 项奖励
1 解答
878 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Maksym

in general you are right, for mmc numbering please refer to

Table 30. Linux uSDHC relationships attached Linux Guide.

Also may be recommended to post it on uboot mail list.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
879 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Maksym

in general you are right, for mmc numbering please refer to

Table 30. Linux uSDHC relationships attached Linux Guide.

Also may be recommended to post it on uboot mail list.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------