IMX6 sabresd: mmcblk0 instead of mmcblk2 for SD3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6 sabresd: mmcblk0 instead of mmcblk2 for SD3

Jump to solution
773 Views
maks
Contributor I

Hello all.

I was provided with custom Linux 3.18 kernel. It is not BSP. I could not make it to boot until i changed mmcroot from mmcblk2p2 to mmcblk0p2. However, from user's guide "The SD3 slot uses mmcblk2 on i.MX 6". Is this because of non BSP kernel? Could not find any information to confirm this. I am sorry, just started embedded development.

Labels (2)
0 Kudos
1 Solution
650 Views
igorpadykov
NXP Employee
NXP Employee

Hi Maksym

in general you are right, for mmc numbering please refer to

Table 30. Linux uSDHC relationships attached Linux Guide.

Also may be recommended to post it on uboot mail list.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
651 Views
igorpadykov
NXP Employee
NXP Employee

Hi Maksym

in general you are right, for mmc numbering please refer to

Table 30. Linux uSDHC relationships attached Linux Guide.

Also may be recommended to post it on uboot mail list.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------