IMX6 play special resolution of panel 1920 x 165

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6 play special resolution of panel 1920 x 165

389 Views
VictorWang129
Contributor II

CPU: IMX6 Dual Core

OS: Android 9.0

Here is a special part of my panel. The resolution of the panel is 1920 x 165.

However, it's not a regular panel. Please see the below picture.

This panel is cut from the 17" original panel on the top.

VictorWang129_0-1674111667930.jpeg

VictorWang129_1-1674111703627.jpeg

But the  Vertical Section and Horizontal Section is fit for 17" 1920 x1080.

VictorWang129_2-1674111855119.png

Regarding this, When I play my panel it will show like the below picture. It only show the top of the Android desktop.

VictorWang129_3-1674111918556.png

Could anyone help me with this issue? How can I adjust the desktop to fit this special panel?

 

Tags (1)
0 Kudos
Reply
2 Replies

381 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

You will have to modify the driver since minimum resolution is 320x240 pixels.

Regards

0 Kudos
Reply

365 Views
VictorWang129
Contributor II

Thank you for the reply!

Is that possible to give me some hints about which driver should I modify?

 

0 Kudos
Reply