IMX6 : my DI0_PIN4 doesn't seem to work in GPIO mode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

IMX6 : my DI0_PIN4 doesn't seem to work in GPIO mode

跳至解决方案
949 次查看
patrickauffray
Contributor I

Dear all,

I'm new to the forum and this is my first question, here is the situation : I've developped a specific board from sabresd schematics and Android software with kernel version 3.0.35. On this board i connected a WIFI module (WL1801) whose IRQ pin is linked to DI0_PIN4 pin, i use the others pins of DISP0 connected to a TFT LCD (data + clock+ hsync + vsync + drdy). I've configured DI0_PIN4 as GPIO (MX6DL_PAD_DI0_PIN4__GPIO_4_20) but after booting i notice a stable clock signal on that pin (around 13.5MHz) whatever the pin is configured (i've tested AUD6_RXD & IPU1_DIN0_PIN4 as well) as there was something coming above pin muxing configuration.

Has someone already faced this kind of problem please ?

With my best regards, Patrick.

标签 (3)
0 项奖励
回复
1 解答
670 次查看
igorpadykov
NXP Employee
NXP Employee

Hi patrick

I would suggest to set iomux register using memtool and check once more,

it should work:

Re: TX53 configure gpio pins from c linux code

[Share] How to make memtool accessing the WEIM registers success in iMX25 Linux BSP

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
671 次查看
igorpadykov
NXP Employee
NXP Employee

Hi patrick

I would suggest to set iomux register using memtool and check once more,

it should work:

Re: TX53 configure gpio pins from c linux code

[Share] How to make memtool accessing the WEIM registers success in iMX25 Linux BSP

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复