IMX6 VTT Termination with Pmic100 VREFDDR pin

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6 VTT Termination with Pmic100 VREFDDR pin

742件の閲覧回数
bastien
Contributor I

Hello,

I am working on imx6Q pcb board and I would like to use 4 DDR3 chips in fly-by topology.

In the 3.7§ DDR power recommendations of the Hardware Development Guide, NXP tells about DDR_VTT. I read articles and documentations which specify to use SW4 VTT mode.

I want to use the PMIC0100 chip in default mode.

1_ Does the VTT island can be provided by the VREFDDR pin (pmic)?

Also the number of decoupling capacitor is not clear.

2_ How many decoupling capacitors need to be placed on VTT island?

I saw Open Source project with decoupling capacitor between VTT and GND and between VTT and DDR_1.5V

3_ Did the last decoupling capacitor between VTT and DDR_1.5V is required ?

Hope someone could help me.

Best regards

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 返信

692件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Bastien

I sent example schematic for  4 DDR3 chips in fly-by topology via mail.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信