IMX6 Solo Lite Custom board Pin Multiplexing

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX6 Solo Lite Custom board Pin Multiplexing

1,008 次查看
satyavenkatasan
Contributor I

Dear Freescale,

We are using the IMX6 Solo lite Processor in our design. Using the iomux_tool_v3.4.0.3 we selected the peripherals & pin functionality in the tool and generated the pin muxing .c & .h files. Know I wanted to patch with the IMX6Sl evk 3.0.35 version kernel. hear I have 2 questions is it possible to patch the files that got generated directly. if it so, suggest me the steps. if direct patching is not possible suggest me how can i use this files in detail.

Thanks & regards,

Satya Venkata Sandeep A.

标签 (3)
0 项奖励
回复
1 回复

606 次查看
igorpadykov
NXP Employee
NXP Employee

Hi satya

there is no currently an automated way to transfer a design from iomux

files to linux. One can edit linux files manually using

Chapter 2 Configuring the IOMUX Controller  attached Porting Guide.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复