IMX6 Sabresdb PCIe EP problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6 Sabresdb PCIe EP problem

2,134 Views
rehankhan
Contributor I

HI,

 

I am facing problem in enabling PCIe support on my sabresdb imx6 board. Following are my kernel config and booting logs. I want to enable EP PCIe mode in kernel

 

1) Attaching kernel config file

kernel version is linux-2.6-imx-imx_3.10.53_1.1.0_ga/.

 

2) Boot Log

 

Attaching boot log file.

 

What could be the reason for following error

 

imx6q-pcie 1ffc000.pcie: lvds_gate clock select missing or invalid

imx6q-pcie: probe of 1ffc000.pcie failed with error -2

 

 

Please help

 

Regards,

Rehan Khan

Original Attachment has been moved to: config.zip

Original Attachment has been moved to: log.txt.zip

Labels (1)
0 Kudos
Reply
2 Replies

785 Views
Yuri
NXP Employee
NXP Employee

  Strictly speaking, the i.MX6 Linux supports only PCIe RC mode.
As stated in the next thread,  

“PCIe host controller driver in 3.10.17 kernel”

https://community.freescale.com/message/423867#423867

“Did you enable RC or EP option in the kernel configuration when build the kernel image?

These two options are only used in imx6 pcie ep/rc validation system, please disable them
if they are enabled in your kernel configuration. Otherwise, imx6 pcie wouldn't work properly.”

The next is link for “i.MX6Q PCIe EP/RC Validation System” thread :

https://community.freescale.com/docs/DOC-95014


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

785 Views
rehankhan
Contributor I

Hi,

So I assume that we cannot use IMX6 in PCIe EP mode. Will we get further support on this issue?

0 Kudos
Reply