IMX6 Sabre board - USB Host Mode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX6 Sabre board - USB Host Mode

771 次查看
jhtate1
Contributor I

Hello support,

We need 2 USB ports, one is for android debugging and one is for mouse or touch controller connected.  

How can we install the USB host device on top of IMX6 Sabre board.

Also we need to know how to change the linux kernel to enable imx6’s usb host.

Thank you

标记 (3)
0 项奖励
1 回复

488 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  Please refer to Linux documentation about USB :

Chapter 10 of “i.MX_BSP_Porting_Guide.pdf” ;

Chapter 39 (CHIPIDEA USB Driver) of “i.MX_Linux_Reference_Manual.pdf”.

 

http://www.nxp.com/webapp/Download?colCode=L4.1.15_1.2.0_LINUX_DOCS

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励