Hi,
We are using imx6q chipset having PCIe based Gigabit Ethernet Link , In which we are not able to produce higher throughput even having the possibility upto 2.5 Gbps . If we are using MTU more than 400 we are finding packet loss and packet drop in the data transmission.
Processor - imx6q
PCIe to LAN - RTL8111F-CG (RT8169 device driver).
Would be really helpful for response.
解決済! 解決策の投稿を見る。
Hi
I found the problem for the PCIe low throughPut Bug. When we are using 4.9 kernel , r8169.c driver is having problem with the MRRS(max read request size) of the PCIe is being set to 4096 . By this the over all link is getting dropped .
Solution : Set the MRRS size to 512 or we can disable the rtl_tx_performance_tweak function will solve the problem in 4.9 version kernel . And In 5.4 kernel the updated r8169_main.c driver is not having this problem.
Thanks ,
Abhishek
Hi
I found the problem for the PCIe low throughPut Bug. When we are using 4.9 kernel , r8169.c driver is having problem with the MRRS(max read request size) of the PCIe is being set to 4096 . By this the over all link is getting dropped .
Solution : Set the MRRS size to 512 or we can disable the rtl_tx_performance_tweak function will solve the problem in 4.9 version kernel . And In 5.4 kernel the updated r8169_main.c driver is not having this problem.
Thanks ,
Abhishek