We use Samsung and Micro 2Gb DDR3 on IMX6/Q , no problem , now change to 4Gb Hynix DDR3 H5TQ4G63AFR-PBC (256MX16), total is 2GBYTE, Mfgtool hanging in load U-BOOT.
we make 10PCS board, each board has the same problem. after replace the Hynix 4Gb DDR3 with the Micron 2Gb DDR3, program is OK.
please advise how to fix
"
DLL version: 2.2.3
Tuesday, December 24, 2013 22:50:11 Start new logging
ModuleID[2] LevelID[10]: CMyExceptionHandler thread is running
ModuleID[2] LevelID[1]: new MxHidDeviceClass
ModuleID[2] LevelID[10]: new MxHidDevice[0173FBE8]
ModuleID[2] LevelID[10]: Device Manager thread is running
ModuleID[2] LevelID[10]: CmdOperation[0] device chagned and reset to state 0
ModuleID[2] LevelID[10]: ExecuteCommand--Boot[WndIndex:0], File is D:\Mfgtools-Rel-4.1.0_130816_MX6Q_UPDATER\Mfgtools-Rel-4.1.0_130816_MX6Q_UPDATER\Profiles\MX6Q Linux Update\OS Firmware\u-boot-mx6q-sabresd.bin
ModuleID[2] LevelID[10]: ExecuteCommand--Load[WndIndex:0], File is D:\Mfgtools-Rel-4.1.0_130816_MX6Q_UPDATER\Mfgtools-Rel-4.1.0_130816_MX6Q_UPDATER\Profiles\MX6Q Linux Update\OS Firmware\uImage, address is 0x10800000
ModuleID[2] LevelID[10]: PortMgrDlg(0)--Command Load excute successfully, retry count: 0
ModuleID[2] LevelID[10]: ExecuteCommand--Load[WndIndex:0], File is D:\Mfgtools-Rel-4.1.0_130816_MX6Q_UPDATER\Mfgtools-Rel-4.1.0_130816_MX6Q_UPDATER\Profiles\MX6Q Linux Update\OS Firmware\initramfs.cpio.gz.uboot, address is 0x10C00000
ModuleID[2] LevelID[10]: PortMgrDlg(0)--Command Load excute successfully, retry count: 0
ModuleID[2] LevelID[10]: ExecuteCommand--Jump[WndIndex:0]
ModuleID[2] LevelID[10]: *********MxHidDevice[0173FBE8] Jump to Ramkernel successfully!**********
ModuleID[2] LevelID[10]: CmdOperation[0], current state command has been finished and the last command is successful, so SetEvent(hDevCanDeleteEvent)
已解决! 转到解答。
Hi Gavin,
Could you please download excel file from i.Mx6DQSDL DDR3 Script Aid ?
You can base on this xls file to setting your DRAM timing first.
Hi Gavin,
(1)
Do you have update yout Mfgtools-Rel-4.1.0_130816_MX6Q_UPDATER\Profiles\MX6Q Linux Update\OS Firmware\u-boot-mx6q-sabresd.bin to 4Gbit setting ?
(2)
Do you have use DDR_STRESS_TOOL to check your DRAM setting is correct and stable ?
Hi Apollo:
we use DDR_STRESS_TOOL check , the maximum speed can only run at 475MHz, and we set the DDR clock to 400Mhz , MFGtool is OK to finish program.
But I wish to know how to tune the clock to 528MHz.
thanks
Hi Gavin,
Which CPU your using ?
Base on MFGTOOL , Are you using MCIMX6Q CPU ?
If you using i.MX6Q CPU , we suggest pass 600MHz via DDR_STRESS_TEST tool base on 2Gbit board.
Do you have send your layout file to local FAE to check again ?