IMX6 - IPU Warning - IPU_INT_STAT_10 = 0x00080000

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6 - IPU Warning - IPU_INT_STAT_10 = 0x00080000

2,270件の閲覧回数
manoelramon
Contributor I

Hi

   I am seeing the following message during the boot:

imx-ipuv3 imx-ipuv3.0: IPU Warning - IPU_INT_STAT_10 = 0x00080000

  According to the reference manual for IMX6 this is releated to "display controller error channel 1" when the anti tearing effect is enabled.

  Do you have idea how I can fix this ? I am using Android

ラベル(4)
0 件の賞賛
6 返答(返信)

1,382件の閲覧回数
manoelramon
Contributor I

I will try.. but do you know ? it is odd.. I noticed this warning appears sometimes.. how come ?

0 件の賞賛

1,382件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

also may be recommended to decrease bus loading (for example

reduce lcd fps or resolution) and avoid to use IPU IC.

Best regards
igor

0 件の賞賛

1,382件の閲覧回数
manoelramon
Contributor I

Hello

   Please someone has any insight ?

I am using the following command line:

Kernel command line: console=ttymxc0,115200 init=/init video=mxcfb0:dev=lcd,Newhaven-LCD,if=RGB24,bpp=32 fbmem=28M fb0base=0x27b00000 vmalloc=400M androidboot.console=ttymxc0 androidboot.hardware=intrinsyc no_console_suspend=1 dmfc=3

however, the IPU warning happens sometimes only.

0 件の賞賛

1,382件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Manoel

please try the 'dmfc=3' kernel boot-up command option. This would increase display FIFO size.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛

1,382件の閲覧回数
manoelramon
Contributor I

Igor

   False alarm.. I still have 

imx-ipuv3 imx-ipuv3.0: IPU Warning - IPU_INT_STAT_10 = 0x00080000

Can you clarify what dmfc means ?

0 件の賞賛

1,382件の閲覧回数
manoelramon
Contributor I

Igor

   Many thanks!!! worked very well!

Regards

0 件の賞賛