IMX6 HDMI I2C bus

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6 HDMI I2C bus

Jump to solution
1,022 Views
Kazuma_Sasaki
Senior Contributor I

Community and hardware design guide mentioned that IMX6 should be use dedicated I2C(DDC_SCL/DDC_SDA).

We would like to use other I2C bus due to our system design. Please let me confirm several points with you.

Q1. I suppose we can use other I2C bus (I2C1 or I2C3) for HDMI if we do not need HDCP feature. Is it right?

Q2. I suppose we do not need I2C bus for HDMI if HDMI driver has EDID information statically. Is it right?

       Because, our system always connect to same display. does not need getting DTD information from display via I2C.

From community

IMX6 - HDMI I2C bus 

From hardware design guide

pastedImage_2.png

Best Regards,

Kazuma Sasaki.

Labels (2)
0 Kudos
1 Solution
813 Views
igorpadykov
NXP Employee
NXP Employee

Hi Kazuma

>Q1. I suppose we can use other I2C bus (I2C1 or I2C3) for HDMI if we do not need HDCP feature. Is it right?

right

>Q2. I suppose we do not need I2C bus for HDMI if HDMI driver has EDID information statically. Is it right?

yes it is right.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
2 Replies
814 Views
igorpadykov
NXP Employee
NXP Employee

Hi Kazuma

>Q1. I suppose we can use other I2C bus (I2C1 or I2C3) for HDMI if we do not need HDCP feature. Is it right?

right

>Q2. I suppose we do not need I2C bus for HDMI if HDMI driver has EDID information statically. Is it right?

yes it is right.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
813 Views
Kazuma_Sasaki
Senior Contributor I

Hi Igor,

I appreciate you support. I got it.

Best Regards,

Kazuma Sasaki.

0 Kudos