Hello,
I am designing a product that has an IMX6 processor in an FCPBGA package. The main PCB is mounted in an aluminum enclosure, which I would also like to use as a heatsink for the IMX6.
A thermal gap pad is placed between the enclosure and the IMX6 for optimal heat transfer. The pad is kept in place by the pressure of the case on the PCB. I have mechanical information about the pad (hardness, thickness, Young's Modulus), but I don't know how much pressure can be applied on the FCPBGA package.
Is there any information available from Freescale regarding about the maximum pressure that can be applied without damaging the package?
解決済! 解決策の投稿を見る。
Hi Sammy
maximum pressure is described on p.44 FCPBGA presentation
http://cache.freescale.com/files/32bit/doc/package_info/FC-PBGAPRES.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Sammy
maximum pressure is described on p.44 FCPBGA presentation
http://cache.freescale.com/files/32bit/doc/package_info/FC-PBGAPRES.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Alright so anything below 45N should be acceptable? I assume PoP versions of the IMX6 are a bit more fragile, or can they handle the same pressure?