IMX537 video problem under WINCE7 BSP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX537 video problem under WINCE7 BSP

633件の閲覧回数
zhuyiwu
Contributor I

  We have a IMX537 board with a ADV7180BSTZ chip. The WINCE7 BSP has been successfully installed, everything goes well except the video function. We found:

  1, When CSI0 mode is set to "interlaced", there is no video output, also no IDMAC_EOF_0 interrupt is triggered.

  2, When CSI0 mode is set to "progressive", the images flap upward and unstable.

  3, When CSIO mode is set to "Gated Clock", the images are horizental mirrored.

  the following list is the setting of CSI0 registers:

                                    CSI 0 Registers

        PID:00400002 TID:04D2004A Address d5290000  04008a30 027002cf 023f02cf 00000000

        PID:00400002 TID:04D2004A Address d5290010  00000000 000d07df 00040596 00ff0000

        PID:00400002 TID:04D2004A Address d5290020  ffffffff 00000000 00000000 00000000

        PID:00400002 TID:04D2004A Address d5290030  00000000 00000000 00000000 00000000

        PID:00400002 TID:04D2004A Address d5290040  00000000 00000000 00000000 00000000

        PID:00400002 TID:04D2004A Address d5290050  00000000 00000000 00000000 00000000

  Same video chip has been tested on the IMX357 board under WINCE6 environment without any problem.

  For this, any one with any luck in IMX537?

  BTW, could anyone explain the CSIO CCIR Code Register 1 ( IPU_CSI0_CCIR_CODE_1 ) to me? there is no detail explanation in the manual, such as the fields of:

       CSI0_STRT_FLD0_ACTV

       CSI0_END_FLD0_ACTV

       CSI0_STRT_FLD0_BLNK_2ND

       CSI0_END_FLD0_BLNK_2ND

       CSI0_STRT_FLD0_BLNK_1ST

       CSI0_END_FLD0_BLNK_1ST

ラベル(1)
タグ(2)
0 件の賞賛
1 返信

498件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

Please check my captured images for the register.

Regarding this issue " When CSI0 mode is set to "progressive", the images flap upward and unstable"

Would you please adjust the value of "CSI0_VSC" in the "IPU_CSI0_OUT_FRM_CTRL" register.

12689_12689.jpgCapture1.JPG.jpg12690_12690.jpgCapture2.JPG.jpg