IMX53 change DDR3 from 1333 to 1666

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX53 change DDR3 from 1333 to 1666

1,129 次查看
xiaoxiongdeng
Contributor II

Hi,all

     Recently, we have changed imx53's DDR from DDR3-1333 to DDR3-1666. I had some questions about the ESDCTL setting in  imx53RM.pdf.

    for example:

               the ESDCTL_ESDOTC register, bit[29-27]:tAOFPD, the unit is cycle ; but bit[23-20] tANPD, the unit is clock .

               I don't konw what is the different between    cycle   and    clock .

  who can help me !

     thanks !

标签 (3)
标记 (3)
4 回复数

853 次查看
gusarambula
NXP TechSupport
NXP TechSupport

The tANPD delay is also in clock cycles even though the cycle/clock difference on this register’s bit definitions may cause confusion.

853 次查看
xiaoxiongdeng
Contributor II

Hi

     I have another question about imx53 DDR3 debug. the ESDCTL_ESDREF register ,bit [15,14] - Refresh Selector, how can I select 64KHz or  32 KHz . I can not find somewhere to explain that .

     thanks !

0 项奖励
回复

853 次查看
gusarambula
NXP TechSupport
NXP TechSupport

You would need to select this value depending on the required periodic refresh rate (tREFI) of the memory being used. There are a couple of tables you may use as reference in sections 28.5.4 and 28.121.9 of the Reference Manual.

Please note that the DDR controller of the i.MX53 supports x16/x32 DDR3 memories up to 400MHz (800 MHz data rate).

853 次查看
xiaoxiongdeng
Contributor II

HI , gusarambula

     thanks for your help !

     But I have another question ,  because i.MX53 support DDR3 memories only up to 400M(800Mhz data rate), so if we use DDR3-1333 or DDR3-1600 memories, the timing parameters we should set to adjust to DDR3-800 , instead of DDR3-1333 or DDR3-1600.

     Is my thinking right?

    

     thanks!