Dear Freescale.
I have question IMX28 Board current issue after mem mode.
We are testing to standby mode and mem mode on IMX28 board.
In cpu clock 454MHz case, idle status board current is 86mA.
But , Entry to mem mode and after wake up board, board current is 94mA.( more up to 10%)
i want know Why that increase power current??
what is difference befor mem mode and after mem mode?
customer project is mobile phone application., so power consumption is very important.
please help us.
thanks.
Hi Freescale
Current CPU clock value is same 454.736(454.736MHz) - befor and after mem mode.
Customer is had some point jumper on IMX28EVK, so we successed test mem mode.
please check to this current issue.
thanks
Hi Sung-Uk,
just small remark below: :smileyhappy:
so called "mem mode" is not real low power mode, because
really i.MX28 is completely powered down, while state of its main
modules [really not all], CLKCTRL, PinCtrl are saved in DDR memory
[so called "context"]. From sect.3.6.2 "Suspend-To-RAM mode "
AN4199 Using the i.MX28 Power Management Unit and Battery Charger:
"In this mode, the i.MX28 is placed in the Power-Off state. The DRAM is placed in the Self-Refresh state,
and all the context and register values are stored in the DRAM to allow the device to wake up quickly on
resume. As the i.MX28 is in Power-Off state, the DC-DC converter is not active. Therefore, an external
power supply is needed for the DRAM. Only PSWITCH can be used to wake up the device from
Suspend-To-RAM mode."
Practical consequence from this solution is next: for example some device is
active after OS start-up. Then your application wisely decided to turn it off just before
entering "mem mode". However after exit from "mem mode" you will see that it is still
active and current is more, then just before entering "mem mode". This happened because
you should save in "context" state of this device. Exit from "mem mode" is cold start-up
event with restoring only data, which one saved in "context".
So suggestion to check what is saved in your "context", this depends on particular
application.
Best regards
chip
hi,Sung-UK
sorry to interrupt you
I have a mem-mode problem ------ suspend to ram wakeup fail
could you send me informations about how to do mem-mode test ( configure,build 、test)
please help me out
Briefly:
in "mem mode" you take responsibility
in software to restore processor state to original
(before entering "mem mode") - only in this case
you will get the same power figures (before and after "mem mode").
Hi Sung-Uk
I believe some peripherals connected to processor
may cause such consumption.
Please try to measure i.MX28 currents,
for example on i.MX28 EVK with Freescale Linux BSP:
echo standby > /sys/power/state
VDDD 10mA
VDDIO 15mA
VDDA 5mA
Also it may be recommended to try measurements with board
without populated external components.
Best regards
chip
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Sung-Uk
sorry what do you mean by "mem mode" ?
In the original EVK design (i.MX28 EVK), DRAM power source is provided by the
on-chip power supply and it will be turned off during mem mode.
In order to support suspend to RAM, it must be connected to a constantly
on power source rather than the on-chip power supply.
So "mem mode" can not be tested on i.MX28 EVK.
Probably " IMX28EVM board" as you calls it - something else, not i.MX28 EVK.
So suggestion - please try measurements with board
without populated external components.
Best regards
chip