IMX278 camera for I.MX6 custom board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX278 camera for I.MX6 custom board

537 Views
alexandrechartr
Contributor II

Hello,

We are currently developing a custom board and we would like to add an IMx278 camera. The camera use the CSI interface with 4 lanes.

I would line to know if someone is aware of any available driver for this camera? If not, is there any similar driver witch I can reuse to make my own?

Thank you,

Labels (3)
0 Kudos
1 Reply

371 Views
igorpadykov
NXP Employee
NXP Employee

Hi Alexandre

one can start with Debug steps for customer MIPI sensor
https://community.freescale.com/docs/DOC-94312

AN5305 MIPI-CSI2 Peripheral on i.MX6 MPU
http://cache.nxp.com/files/32bit/doc/app_note/AN5305.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos