When my system is wake up from sleep mode sometime I can not get the right picture from Camera ( RAW Data from camera I/F ). Should be the Camera Clock not Sync with iMX.
I use the IMX25 & IMX6SL , Both CPU have the same problem. You can see the image as attach.
How can I avoid this problem ?
Hi Johnson
for i.MX25 please implement workaround for
ENGcm12381 CCM: PLL locks at lower frequency when returning from a low power
mode, IMX25CE Chip Errata for the i.MX25
<ltib_dir>/rpm/BUILD/linux/arch/arm/mach-mx25/system.c
For i.MX6SL use latest BSP with all latest fixes
L3.0.101_4.1.1_SOURCE_BSP : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite,
i.MX 6Solo and i.MX 6Sololite Linux BSP Source Code Files.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------