IMX issues with HDQ driver (bad battery readings)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX issues with HDQ driver (bad battery readings)

776件の閲覧回数
manoelramon
Contributor I

Hi

   We are using HDQ I/O to communicate with our battery. What we noticed is the IMX sometimes reads a lot of bad values from the battery informing wrong capacity and temperature which makes our device to power down.

   We are using HDQ I/O, in other words, using a GPIO, and when we have WiFi ON, the performance is significantly worst, in other words, the incidence of wrongs readings is higher.

   I was taking a look in the driver, and the implementation has a bunch of microsecond delays. Is this an issue because Linux is not RTOS and we cannot guarantee the performance of GPIOs ? I was thinking the microdelays which has dependencies of jiffies, actually might be impacted when the power govern is changed (interactive, conservative, etc).

   Please let me know what you guys think, and of course, thank you very much!

ラベル(5)
0 件の賞賛
返信
2 返答(返信)

632件の閲覧回数
manoelramon
Contributor I

Igor

  Thanks... Actually I discovered the problem. The driver was using gpio configuration function calls all the time instead the simple gpio set and read calls.

  With the change I had a much clear hw signal and an optimal performance. I also changed some timing for HDQ.

Thanks!

Manoel

0 件の賞賛
返信

632件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Manoel

errors may be caused by noise so one can check signals

with oscilloscope. From software point of view one can try to

run code on separate core if this is multicore processor.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信