IMX issues with HDQ driver (bad battery readings)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX issues with HDQ driver (bad battery readings)

773 Views
manoelramon
Contributor I

Hi

   We are using HDQ I/O to communicate with our battery. What we noticed is the IMX sometimes reads a lot of bad values from the battery informing wrong capacity and temperature which makes our device to power down.

   We are using HDQ I/O, in other words, using a GPIO, and when we have WiFi ON, the performance is significantly worst, in other words, the incidence of wrongs readings is higher.

   I was taking a look in the driver, and the implementation has a bunch of microsecond delays. Is this an issue because Linux is not RTOS and we cannot guarantee the performance of GPIOs ? I was thinking the microdelays which has dependencies of jiffies, actually might be impacted when the power govern is changed (interactive, conservative, etc).

   Please let me know what you guys think, and of course, thank you very much!

0 Kudos
Reply
2 Replies

629 Views
manoelramon
Contributor I

Igor

  Thanks... Actually I discovered the problem. The driver was using gpio configuration function calls all the time instead the simple gpio set and read calls.

  With the change I had a much clear hw signal and an optimal performance. I also changed some timing for HDQ.

Thanks!

Manoel

0 Kudos
Reply

629 Views
igorpadykov
NXP Employee
NXP Employee

Hi Manoel

errors may be caused by noise so one can check signals

with oscilloscope. From software point of view one can try to

run code on separate core if this is multicore processor.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply