IMX clock domain

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX clock domain

645 Views
justinfei
Contributor I

When I read the datesheet of IMX8mq about the CCM.

1.I can't understand the clock domain usage and why the same clock have 4 domain setting(for example CCM_PLL_CTRLn has setting1 ~setting3).The 4 domain settings of one clock are working at the same time?

2.What is the usage of PLL domain settings and CCGR domain settings?

em......NXP's datasheets are hard to understand!

0 Kudos
2 Replies

334 Views
tamotsu
Contributor III

Hi.

I also didn't understand that there are 4 domains.

"3.2.1.1 Features" of Resource Domain COntroller(RDC) in i.MX7D reference manual written as follews.

Assignment of cores, bus masters, peripherals, and memory regions to a resource domain.

Four of these ?

But it dosen't write which one is domain0.

0 Kudos

633 Views
igorpadykov
NXP Employee
NXP Employee

Hi

 

for domain usage one can look at description in sect.5.1.5.7 Access control, sect.5.1.6.2 PLL Interface,

sect.5.2.4.2 Low power mode

i.MX 8M Dual/8M QuadLite/8M Quad Applications Processors Reference Manual

 

Best regards
igor

0 Kudos