IMX 6D6A fail to boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX 6D6A fail to boot

414 Views
Makabaka
Contributor II

Hi :

I made some boards using IMX6D6A(D version) and the boot mode was configured as external parallel Norflash , but one of the boards failed to boot.

 

Using serial download mode(boot mode[1:0]),  can debug in RAM mode, and read SRC_SBMR1 is 00000000, SRC_SBMR2 is 30000001.This is not the right value.

Test power supply, crystal oscillator is OK.The problem persisted after replaced a new CPU.

Could you please help to analyze the reasons for this phenomenon?

0 Kudos
1 Reply

405 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ziv5

 

for SRC_SBMR1,2 wrong values one can check power-up sequence using

oscilloscope and try to prolong POR duration (just for test up to 1sec.), also

may be recommended to check both crystals (24MHz, 32.768KHz).

As reference please use IMX6DQ6SDLHDG, Hardware Development Guide for i.MX 6Quad, 6Dual, 6DualLite, 6Solo Families of Applic...

 

Best regards
igor

 

0 Kudos