I'm using i.MX6Q
and linux version is 3.0.35
My sound codec(ALC5629) connect throgh SD2_DAT0, SD2_DAT1, SD2_DAT2, SD2_DAT3
below is ssi port setting in board-mx6q_sabresd.c
---
static struct mxc_audio_platform_data alc5629_data = {
.ssi_num = 1,
.src_port = 2,
.ext_port = 4,
.init = mxc_alc5629_init.
};
---
and below is GPIO port setting in board-mx6q_sabresd.h
---
MX6Q_PAD_SD2_DAT0__AUDMUX_AUD4_RXD, //ADCDAT
MX6Q_PAD_SD2_DAT1__AUDMUX_AUD4_TXFS, //LRCK
MX6Q_PAD_SD2_DAT2__AUDMUX_AUD4_TXD, //DACDAT
MX6Q_PAD_SD2_DAT3__AUDMUX_AUD4_TXC, //BCLK
---
when playback wav file using aplay
no sound output and no signal that port(check using osciloscope)
how can i fix this problem?
解決済! 解決策の投稿を見る。
Hi hyunho
please check Chapter 8 Porting Audio Codecs to a Custom Board
attached Porting Guide document.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi hyunho
please check Chapter 8 Porting Audio Codecs to a Custom Board
attached Porting Guide document.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
when play wav file using aplay. aplay is blocked
so i think pcm device is not working..
how can i check about this problem?