Hi Experts,
We have an sensor connected to I2c3 of the IMx6sl board. I have to use i2c3 in master mode and sensor in Slave mode.I have made the necessary changes to dtb file and i can see device being probed.
root@imx6slzbha:~/system_init# cat /sys/class/i2c-dev/i2c-0/name
21a8000.i2c
mailto:root@imx6slzbha:~/system_init#
My Test Code:-
#define SLAVE_ADDR 0xD6
#define I2C_DEVICE "/dev/i2c-0"
int main(int argc,char **argv) {
int dev;
unsigned char res,res2;
int temperature ;
if ((dev = open(I2C_DEVICE, O_RDWR)) < 0){
perror("open failed");
exit(1);
}
if (ioctl(dev, I2C_SLAVE, SLAVE_ADDR) < 0){
perror("ioctl failed");
close(dev);
exit(1);
}
res = i2c_smbus_read_byte_data(dev, WHO_AM_I_M);
printf("Result= %d\n\r\n\r", res);
close(dev);
exit(0);;
}
I am getting error :- ioctl failed: Invalid argument
Can someone please guide me where I am wrong .
Regards
Sandeep S
Hi Sandeep
one can try to debug it, which function and what argument causes such error using
Chapter 35 Inter-IC (I2C) Driver attached Linux Manual.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------