I want to install v4l2_h264 for imX8

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I want to install v4l2_h264 for imX8

1,164 Views
santhosh2
Contributor IV

Hello , everyone !

I want to install v4l2_h264 for imX8 but while running command -> " gst-launch-1.0 -e v4l2src device=/dev/video3 ! videoconvert ! x264enc ! mp4mux ! filesink location=test.mp4 "  i get the following error:-

erroneous pipeline: no element "x264enc".

Please provide input .

Thanks and regards,

Santhosh.K

0 Kudos
1 Reply

881 Views
igorpadykov
NXP Employee
NXP Employee

Hi Santosh

available i.MX8 plugins are described in Table 16. i.MX GStreamer 1.0 plugins
attached Release Notes. For i.MX8QM/QXP

one can look at unit test examples linux-test/test/mxc_v4l2_vpu_test/*  , 

mxc_v4l2_vpu_test\test - imx-test - i.MX Driver Test Application Software 

imx-gst1.0-plugins

imx-gst1.0-plugin - i.MX Gstreamer 1.0 Plugin 

More details can be found in Linux L4.14.78_1.0.0 Documentation

in particular sect.6.7 Video Processing Unit (VPU) Linux Manual,

Table 3. BSP and Multimedia standard packages Release Notes.

 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos