I can't confirm that weather this board have an apple I2C Authentication chip. And how can I test it?
1, Is this board have an apple I2C Authentication chip?
2, Which is Authentication chip device in /dev folder?
3, The kernel we use is 3.0.35, If this version kernel support USB DUAL role?
4, If there is a patch for USB DUAL role? After patch to kernel, How to test this board is support USB dual role?
Thanks for any help!
Hi Larry,
Regarding questions 1 & 2:
The i.MX6 SABRE AI board is capable of running CarPlay as shown in the attached document, but the detailed answers you are looking for are restricted to Made For iPod (MFi) licensees, and we will have to provide them to you directly. So, if you need additional details, please submit a Service Request.
Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks for your reply, that is what I want to know. But I confused with “MFi module”, It's software or hardware?
The photo in the attachment, Could you take a full photo include iphone, RCA audio Cable and Speaker?
We want to know more about Carplay and MFi. Please tell me how to submit a Service Request.
Hi Larry,
You could create a Service Request at the link below:
After creating a SR, please post here the SR number.
Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Carlos,
Here is the Service Request, Please give me more details about how to run Carplay on i.MX6 processor.
Service Request Detail
The current status for Service Request number 1-4047193729 is :
Created Date:
(format YYYY-MM-DD HH24:MI:SS) 2015-09-10 00:28:24 GMT
Modified Date:
(format YYYY-MM-DD HH24:MI:SS) 2015-09-10 00:28:24 GMT
Closed Date:
(format YYYY-MM-DD HH24:MI:SS) -
Status: Unassigned
Category: Software Product Support
Topic: Other SW Development Tool
Device Area: ARM Processors
i.MX Applications Processors based on ARM Cores
i.MX 6 Processors
i.MX6D
-
-
Tool/SW name: Carplay MFi module
Tool/SW version: -
Host OS: Linux
Patches installed: -
Severity: Medium
Subject: Carplay MFi module, i.mx6 Dual
Description: The i.MX6 SABRE AI board is capable of running CarPlay, but the
detailed information we are looking for are restricted to Made For iPod (MFi)
licensees. So I submit this service request.
Base Board: MCIMXABASEV1
CPU Cards: MCIMX6DLAICPU1
Display: MCIMX-LVDS1
We want to know:
1, Is this board has an Apple Authentication chip?
2, How can we get "MFi module" and run the Carplay demo?
3, More details about Carplay and MFi.
Thanks for any help!
Notification List: (Update<https://www.freescale.com/webapp/servicerequest.sr_cclist.framework?CLR_SR_ID=1-1UXLEO1>)
Best regards!
Larry
Hi Larry,
I have directed you SR to the experts. Any additional details must be discussed trough that channel and must not be placed on public places according with Made MFi licenses.
Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Carlos,
On i.mx6 linux, which complier can be used?
I use ds-5 Community Edition, does not have a complier.
Best Regards,
Larry
发件人: CarlosCasillas
发送时间: 2015年9月10日 9:06
收件人: Larry cai
主题: Re: - I want do some work about Carplay, Weather this feature is support on this board?
<http://jiveon.jivesoftware.com/mpss/c/iAA/PDcDAA/t.1qb/uKLxlZtMRMeLSu0kRnoFow/h0/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bQ-3D>
I want do some work about Carplay, Weather this feature is support on this board?
reply from CarlosCasillas <http://jiveon.jivesoftware.com/mpss/c/iAA/PDcDAA/t.1qb/uKLxlZtMRMeLSu0kRnoFow/h1/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bQPeieHwSBwpgiZw4FaVMAD4RVzYiZS-2FFh0-2FDND04uTe4umzRv7VSYFy4De7TlVlbw-3D> in i.MX Community - View the full discussion <http://jiveon.jivesoftware.com/mpss/c/iAA/PDcDAA/t.1qb/uKLxlZtMRMeLSu0kRnoFow/h2/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bRdhfuXvs7ZDgxDLvktlmV35kwovANBrZqNQfZRQ-2FZqpQF57CXxz7aDloAAk-2FsgjmI-3D>
Hi Larry,
I was informed that you were already contacted directly, so, no additional information will be posted here. If you have additional questions regarding different topics, we encourage you to create new threads.
Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Carlos,
Thanks for your help, Where do you live, and your work time is?
I’m in china, GMT +08.
Best Regards,
Larry
发件人: CarlosCasillas
发送时间: 2015年9月10日 9:06
收件人: Larry cai
主题: Re: - I want do some work about Carplay, Weather this feature is support on this board?
<http://jiveon.jivesoftware.com/mpss/c/iAA/PDcDAA/t.1qb/uKLxlZtMRMeLSu0kRnoFow/h0/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bQ-3D>
I want do some work about Carplay, Weather this feature is support on this board?
reply from <http://jiveon.jivesoftware.com/mpss/c/iAA/PDcDAA/t.1qb/uKLxlZtMRMeLSu0kRnoFow/h1/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bQPeieHwSBwpgiZw4FaVMAD4RVzYiZS-2FFh0-2FDND04uTe4umzRv7VSYFy4De7TlVlbw-3D> CarlosCasillas in i.MX Community - <http://jiveon.jivesoftware.com/mpss/c/iAA/PDcDAA/t.1qb/uKLxlZtMRMeLSu0kRnoFow/h2/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bRdhfuXvs7ZDgxDLvktlmV35kwovANBrZqNQfZRQ-2FZqpQF57CXxz7aDloAAk-2FsgjmI-3D> View the full discussion
Hi Larry,
I have consulted with the experts regarding questions 1 & 2; you should receive an update soon.
Regarding questions 3 & 4, L3.0.35 already includes USB dual-role (on the OTG port). So, for using the i.MX as Device, the ID pin from micro USB connector must be left floating. When using the i.MX as Host, the ID pin must be grounded.
Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------