Dear All,
I tried to create a yocoto development environment for i.MX6 and i.MX8. The Ubuntu revision is 16.04 LTS, and I follow up i.MX Yocto Project User's Guide (Rev.L4.14.98-2.0.0_ga, 04/209)
However, the 1st bitbake got wrong, Parsing recipes always appear 99% over 1 day.
The 2nd build, there are 5 WARNING and 1 ERROR messages and bitbake process was be interrupted.
Can anyone give me advice? please refer to attached files that you can go over the history.
已解决! 转到解答。
Hi Anderson Hu,
Try to execute this command and build again:
$ sudo pip3 install typing
If you haven't installed it yet, let install it.
Best regards,
Toan
In your second run, you got a memory allocation error [Errno 12] Cannot allocate memory. If you are on a virtual machine, try increasing the amount of RAM allocated to it or increase the swap size. Also if you have any running applications that consume too much RAM, try shutting them down.
Hi turker@dtsis.com,
Yes, I use vmware, and I try to shut down and re-allocate to 8GB RAM, but bitbake problem still exists, but different error and wrong messages.
Anderson Hu
Hi Dao Van Toan,
We have followed the same steps as given by the Anderson Hu and we are able to build successfully with same distro using ubuntu 16.04.
The steps which we have followed are:
$DISTRO=fsl-imx-wayland MACHINE=imx6qsabresd EULA=1 source fsl-setup-release.sh -b build
$bitbake fsl-image-validation-imx
Regards,
Radhika Somaiya.
Hi @Anderson Hu ,
If this is first time you build distro, I recommend that you execute all commands below:
- $ sudo apt-get install gawk wget git-core diffstat unzip texinfo gcc-multilib build-essential chrpath socat libsdl1.2-dev
- $ sudo apt-get install libsdl1.2-dev xterm sed cvs subversion coreutils texi2html docbook-utils python-pysqlite2 help2man make gcc g++ desktop-file-utils libgl1-mesa-dev libglu1-mesa-dev mercurial autoconf automake groff curl lzop asciidoc
- $ sudo apt-get install u-boot-tools
- $ mkdir ~/bin (this step may not be needed if the bin folder already exists)
- $ curl http://commondatastorage.googleapis.com/git-repo-downloads/repo > ~/bin/repo
- $ chmod a+x ~/bin/repo
- $ export PATH=~/bin:$PATH
- $ git config --global user.name "Your Name"
- $ git config --global user.email "Your Email"
- $ git config --list
- $ mkdir fsl-release-bsp
- $ cd fsl-release-bsp
- $ repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-sumo -m imx-4.14.98-2.0.0_ga.xml
- $ repo sync
- $ DISTRO=fsl-imx-x11 MACHINE=imx6ulevk source fsl-setup-release.sh -b build-x11
- $ bitbake fsl-image-gui
But as I can see, you are using Unbutu 16.04 and It's not compatible with build distro <as my experiment>. Something You will get some errors and I dont hard to fix it but It's take time. So I recommend you use unbutu 14.04, It is more compatible with this thing. Good luck.
Best regards,
Toan
Hi Radhika Somaiya and Dao Van Toan ,
I found some information form Yocto Project Reference Manual , you can refer to this web side and the section 1.1.
The Ubuntu 16.4 and Ubuntu 14.4 in supported list. Besides, according to i.MX Yocto Project User's Guide (Rev.L4.14.98-2.0.0_ga, 04/209), the recommended minumum Ubuntu version is 16.04 or later.
In fact, I have re-install Ubuntu 14.04 on vmware workstation, RAM allocation is 8GB, I tried to follow up Dao Van Toan's procedure, but bitbake problem still exists, but the error message is different.
Hi @Anderson Hu,
May you post this error on here? So We can easily analyze and solve it.
And I not ensure that VMware environment will working properly. So I recommend you install dual boot, you also not lag when experience.
Additional info, I build about 10 distros in my computer with no error. It's worth to try, right.
Update: Do you change MACHINE variable in step 15 into your machine.
Hi @Dao Van Toan,
I re-install a clean Ubuntu 14.04 LTS 64bit in VMware and than setup build tools again, I post error message and
log file of failure stored as below.
The Machine variable is imx6qsabresd, I will change Machine variable next step.
Hi Anderson Hu,
Try to execute this command and build again:
$ sudo pip3 install typing
If you haven't installed it yet, let install it.
Best regards,
Toan
Hi toanjunifer@gmail.com and @Tahsin Türker Mutlugün,
Because python 2.7.6 was installed, should I switch python 3 environment by default when I install python 3?
Anderson
Hi anderson_hu0127,
This is a exciting question. Actually, You only need to install it. Don't need to set is as default.
Again, I recommend you install Ubuntu parallel with Windows.
Best regards,
Toan
Hi @Dao Van Toan and @Tahsin Türker Mutlugün,
Thanks for your comments, the build is succeed when installed python3 typing library. Although there are still some warning messages, it has at least succeeded.
Best regards
Anderson
Hi Anderson Hu,
For 1st build: We are able to build for imx6qsabresd (Yocto version 4.14.98_2.0.0). Can you please try to fresh build?
For 2nd build: reason may be insufficient computer memory, free space from your host pc.
Regards,
Radhika Somaiya.
I tried this without problem.
1. $ mkdir imx-yocto-bsp
2. $ cd imx-yocto-bsp
3. $ repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-sumo -m imx-4.14.98-2.0.0_ga.xml
4. $ repo sync
5. $ DISTRO=fsl-imx-x11 MACHINE=imx6qsabresd source fsl-setup-release.sh -b build-x11
6. $ bitbake fsl-image-validation-imx