I.mxrt600 board MIMXRT685-EVK VDDCORE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.mxrt600 board MIMXRT685-EVK VDDCORE

355 Views
Tay
Contributor I

Hello,

I'm trying to work with a vddcore under 1V(0.7, 0.8, 0.9). I choose the frequency and inject the correspondent vddcore value everytime, but whenever the vddcore gets under 1V the system crushes, the program stops running. Can you please guide me how to fix this?

Thanks in advance!!

0 Kudos
1 Reply

339 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
To provide the fastest possible support, I'd highly recommend you to refer to the application note and pca9420 demo in the SDK library.
Have a great day.
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos