I.mx6ul evk critical temperature reached

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

I.mx6ul evk critical temperature reached

632 次查看
vikneshwarthand
Contributor II

Hi,

we are using the I.MX6UL evk board for development.

we pulled the codec MAIN mic bias voltage to 12v externally to test with the external mic and it worked well. but after some time, the board started throwing the message "temperature is exceeding" so immediately we turned it off and tried powering up after some time. again during the bootup, it is throwing  "temperature exceed so shutting down " so we turned off the device and started testing the board for short in the power lines but nothing is found. 

we are stuck. so don't know how to recover the SOM board. so please help us. 

we are attaching the image of the circuit chage we made and debug port message window. please refer to it and reply ASAP .SC_3.pngSC_1.pngSC_2.png@

标签 (3)
1 回复

571 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Vikneshwar

most components are 6.3V rated so they may be damaged by applying 12V.

So there is possibility that processor was also damaged, you can replace it

or cpu/baseboard.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------