I have Sabre board(MCIMX6SX-SDB) from NXP, now require full source code or link to download

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I have Sabre board(MCIMX6SX-SDB) from NXP, now require full source code or link to download

432 Views
anilchowdary
Contributor II

Hi, I have Sabre board(MCIMX6SX-SDB), with this only bootable images but i don't not full source code. So we require the full source code which include toolchain and  A9 and M4 source to compile and build. Please share the source also related links.

Thanks & Regards

-Anil

Labels (1)
0 Kudos
1 Reply

310 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Anil Kumar,

You can build customized images for the i.MX6SX SABRE Board using the Linux BSP Release (link below, please note that you may need to login in order to download this file).

https://www.nxp.com/webapp/Download?colCode=L4.1.15_2.0.0-LINUX-DOCS

Please follow the Yocto User’s Guide document contained in this bundle. Since Yocto is used as a means of distribution the source code is fetched on demand. You may, however, fetch the required sources for a given image by using the following command:

bitbake <image_or_recipe> -c fetchall

You may also extract the toolchain using:

bitbake meta-toolchain

Once fetched you can find the source code on the work directory:

/<BSP_DIR>/<BUILD_DIR>/tmp/work/

For example, the source for the kernel would be on:

/<BSP_DIR>/<BUILD_DIR>/tmp/work/<MACHINE>/linux-imx/<KERNEL_VER>/git/

The sources are located depending on the recipes that compiles and install the packages so it may not be very straightforward.

I hope this information helps! 

 Regards