I don’t know how to set the x, that keyboard drive can be loaded correctly.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I don’t know how to set the x, that keyboard drive can be loaded correctly.

615 Views
guozhongchen
Contributor I

 Freescale development kit provides two options—— Preconfig Min Profile and

FSL gnome release package.

The first option will not compile gtk+gstreamer,and X11lib.

The second option will generate the …… but the file that generates the rootfs directory too large.

I just need the minimum configuration to run gtk application. So I chose the first option——Preconfig Min Profile. And then config the kernel to compile gtk+ libgstreamer lib , and X11.

Because the target board without matrix keyboard, only use the keys of linking GPIO instead. I modify the routine. Adding the configuration code—— gpio_keys_button as follow:

 

#if defined(CONFIG_KEYBOARD_GPIO) || defined(CONFIG_KEYBOARD_GPIO_MODULE)

 

 

static struct gpio_keys_button mx23evk_gpio_buttons[] = {

 

{

 

.gpio = MXS_PIN_TO_GPIO(PINID_SSP1_DETECT),

 

.type = EV_KEY,

 

.code = KEY_A,//KEY_VOLUMEUP,

 

.desc = "SW105",

 

.active_low = 1,

 

.wakeup = 1,

 

},

 

 

 

{

 

.gpio = MXS_PIN_TO_GPIO(PINID_SSP1_DATA0),

 

.type = EV_KEY,

 

.code = KEY_B,//KEY_UP,

 

.desc = "SW108",

 

.active_low = 1,

 

.wakeup = 1,

 

},

 

{

 

.gpio = MXS_PIN_TO_GPIO(PINID_SSP1_DATA1),

 

.type = EV_KEY,

 

.code = KEY_C,//KEY_DOWN,

 

.desc = "SW107",

 

.active_low = 1,

 

.wakeup = 1,

 

},

 

{

 

.gpio = MXS_PIN_TO_GPIO(PINID_SSP1_DATA2),

 

.type = EV_KEY,

 

.code = KEY_D,//KEY_VOLUMEDOWN,

 

.desc = "SW106",

 

.active_low = 1,

 

.wakeup = 1,

 

},

 

{

 

.gpio = MXS_PIN_TO_GPIO(PINID_SSP1_CMD),

 

.type = EV_KEY,

 

.code = KEY_E,//KEY_ESC,

 

.desc = "SW109",

 

.active_low = 1,

 

.wakeup = 1,

 

},

 

 

 

};

 

 

 

 

 

static struct gpio_keys_platform_data mx23evk_gpio_button_data = {

 

.buttons = mx23evk_gpio_buttons,

 

.nbuttons = ARRAY_SIZE(mx23evk_gpio_buttons),

 

};

 

 

 

static struct platform_device mx23evk_gpio_button_device = {

 

.name = "gpio-keys",

 

.id = -1,

 

.num_resources = 0,

 

.dev = {

 

.platform_data = &mx23evk_gpio_button_data,

 

}

 

};

 

 

 

 

 

static void __init mx23_init_gpio_keyboard(void)

 

{

 

platform_device_register(&mx23evk_gpio_button_device);

 

}

 

 

 

 

 

int __init mx23_device_init(void)

 

{

 

 

 

..........

 

..........

 

//add function call in the initialization of device

 

mx23_init_gpio_keyboard();

 

 

 

return 0;

 

}

 

 

 

#endif

 

 

 

And then configure the kernel to enable the GPIO Buttons:

 

 

 

Device Drivers --->

 

Input device support --->

 

[*] Keyboards --->

 

<*> GPIO Buttons

 

 

 

When download the kernel and rootfs to target board. Target board runs and displays:

 

 

 

input: gpio-keys as /class/input/input0

 

input: mxs-kbd as /class/input/input1

 

input: MXS touchscreen as /class/input/input2

 

 

 

Prove gpio-keys driver has been loaded. The information of "printk" prove "input_event" function run correctly.

 

And the function "is_event_supported(type, dev->evbit, EV_MAX)" returns true.

 

 

 

 

 

static void gpio_keys_report_event(struct work_struct *work)

 

{

 

struct gpio_button_data *bdata =

 

container_of(work, struct gpio_button_data, work);

 

struct gpio_keys_button *button = bdata->button;

 

struct input_dev *input = bdata->input;

 

unsigned int type = button->type ?: EV_KEY;

 

int state = (gpio_get_value(button->gpio) ? 1 : 0) ^ button->active_low;

 

/*inkfish debug*/

 

printk(KERN_INFO "%s %s %d\r\n", __FILE__, __FUNCTION__, __LINE__);

 

printk(KERN_INFO "type=%d, button->code=%d, state=%d\r\n", type, button->code, state);

 

input_event(input, type, button->code, !!state);

 

input_sync(input);

 

}

 

 

 

void input_event(struct input_dev *dev,

 

unsigned int type, unsigned int code, int value)

 

{

 

unsigned long flags;

 

 

 

if (is_event_supported(type, dev->evbit, EV_MAX)) {

 

/*inkfish debug*/

 

printk(KERN_INFO "%s %s %d\r\n", __FILE__, __FUNCTION__, __LINE__);

 

 

 

spin_lock_irqsave(&dev->event_lock, flags);

 

add_input_randomness(type, code, value);

 

input_handle_event(dev, type, code, value);

 

spin_unlock_irqrestore(&dev->event_lock, flags);

 

}

 

}

 

 

 

But now I don’t know how to set the x so that keyboard drive can be loaded correctly at the boot.

 

 

Xfbdev -keybd gpio-keys,,device=/dev/input/event0

 

(EE) XKB: Couldn't open rules file /usr/share/X11/xkb/rules/base

 

(EE) XKB: No components provided for device Virtual core keyboard

 

Cannot find keyboard driver gpio-keys

 

The result does not correctly. Why?

 

 

I uploaded my linux kernel config file -- attach Files.

Tags (1)
0 Kudos
Reply
0 Replies