I/O input voltage tolerance

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I/O input voltage tolerance

786件の閲覧回数
robertinant
Contributor I

I need to interface to a i.MX35x processor from a 2.5 volt device.

The i.MX35x I/O Supply voltage is @ 1.8 Volt.

What is the tolerance on the i.MX35x I/O's? e.g. can I directly drive the I/O with 2.5 volt?

Thanks

0 件の賞賛
返信
2 返答(返信)

618件の閲覧回数
david_babin
NXP Employee
NXP Employee

An I/O supplied with 1.8 V cannot be overdriven at 2.5 V. The i.MX35 is similar to other i.MX devices and should not be overdriven > 0.3 V above the associated I/O supply rail. A change ticket will be submitted to correct the data sheet.

0 件の賞賛
返信

618件の閲覧回数
4guin4g4
Contributor IV

According to the Datasheet Table 7

http://cache.freescale.com/files/dsp/doc/data_sheet/MCIMX35SR2CEC.pdf?pspll=1

Supply voltage (I/O) NVCCmax   –0.5  to 3.6 V

0 件の賞賛
返信