I.MX8M Plus Enter JTAG Debug

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I.MX8M Plus Enter JTAG Debug

662件の閲覧回数
hjc
Contributor I

When using NXP I.MX8M Plus chip for bare metal development and debugging, and using DStream emulator to connect to the JTAG interface of I.MX8M Plus processor through JTAG, pin JTAG_ MOD has been set to low level, but the development board cannot enter the JATG debugging mode, and the ROM Table of the chip cannot be read using the J-Link emulator. Does the I.MX8M Plus chip disable the JTAG function when it leaves the factory? How can I enable the Cortex-A53 processor in I.MX8M Plus chip to enter the bare metal debugging mode through JTAG? Thank you

タグ(2)
0 件の賞賛
返信
2 返答(返信)

651件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

 

Yes, JTAG is disable when is leaving the factory, but this is just for rom access you can access to the rest of the code.

 

Regards

0 件の賞賛
返信

646件の閲覧回数
hjc
Contributor I

if i no use rom access, how can i do that use the jtag for debug Cortex-a53 bare metal program ?

how can i do that enter jtag debug mode, thank you

0 件の賞賛
返信