I.MX7S CCM Clko1 Clock gating from kernel space

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX7S CCM Clko1 Clock gating from kernel space

603 Views
akashgajjar
Contributor V

Hi All,

On my i.MX7S board I have configured GPIO1 [02] as Clko1 for feeding clock to the slave device.

At run time from Linux kernel space I need to gate the clock so that can reduce the power consumption.

Is there any mechanism to do that by using sysfs or register level Operation?

Best Regards,

Akash Gajjar 

Labels (2)
0 Kudos
Reply
1 Reply

469 Views
igorpadykov
NXP Employee
NXP Employee

Hi Akash

one can change register value using memtool in unit tests (folder memtool)

imx-test
www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.7.tar.gz

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply