I.MX6UL tools for Secure JTAG mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I.MX6UL tools for Secure JTAG mode

ソリューションへジャンプ
1,190件の閲覧回数
michalkotyla
Contributor II

Hello,

I try to launch imx6UL with secure JTAG mode. In application note AN4686 from 2014, I can see only Lauterbach can support this feature. Is something changed? Is a chance to work in secure mode with any more common tool, like Olimex with OpenOCD?

ラベル(2)
0 件の賞賛
返信
1 解決策
1,135件の閲覧回数
michalkotyla
Contributor II

Hello,
This OpenOCD patch works with Secure JTAG mode. I applied these changes and tested them on code revision 970a12aef with Olimex.

https://review.openocd.org/c/openocd/+/2148/

元の投稿で解決策を見る

3 返答(返信)
1,136件の閲覧回数
michalkotyla
Contributor II

Hello,
This OpenOCD patch works with Secure JTAG mode. I applied these changes and tested them on code revision 970a12aef with Olimex.

https://review.openocd.org/c/openocd/+/2148/

1,122件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

thanks for sharing this useful experience.

 

Best regards
igor

0 件の賞賛
返信
1,153件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Michał

 

one can look at rev.2 2020 AN4686   https://www.nxp.com/docs/en/application-note/AN4686.pdf

there is also support for Arm DS-5/ARMDS DSTREAM debug tool.

 

> Is a chance to work in secure mode with any more common tool, like Olimex with OpenOCD?

 

I am afraid it was not tested on nxp side.

 

Best regards
igor

0 件の賞賛
返信