I.MX6UL Coresight Base address

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX6UL Coresight Base address

1,140 Views
mcbigfoot
Contributor II

Hello,

i'm looking for CoreSight Base address for i.MX6UL.

For orther i.MX6 family devices it was 0x82150000, but it seems to be different for i.MX6UL.

Labels (2)
4 Replies

720 Views
b36401
NXP Employee
NXP Employee

CoreSight base for i.MX6 UL processor is 0x82130000.

I attached you an XML with additional information.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos

720 Views
mcbigfoot
Contributor II

someone?

0 Kudos

720 Views
Yuri
NXP Employee
NXP Employee

Hello,

You may look at IMX6UL.RVC file in the attachments of

the following thread  ARM DS-5 Configuration for i.MX 6UL

Regards,

Yuri.

720 Views
mcbigfoot
Contributor II

Hello,

thanks, but link is not working :smileysad:.

Access to this place or content is restricted. If you think this is a mistake, please contact your administrator or the person who directed you here.